Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
MuNa_4652896
Level 4
Level 4
First like received First like given

Hello

I am compiling a project that incorporates DFU via Bluetooth. The Project compiles successfully with no problems at all. Now, I am merging this project with the original project I am working on, however I am getting this error while merging those files

dfu_mdk_common.h and dfu_mdk_symbols.c

arm-none-eabi-gcc.exe -mcpu=cortex-m0plus -mthumb -I. -IGenerated_Source\PSoC6 -IGenerated_Source\PSoC6\pdl\cmsis/include/ -IGenerated_Source\PSoC6\pdl\devices/psoc6/include/ -IGenerated_Source\PSoC6\pdl\devices/psoc6/include/ip/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/device/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/efuse/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/flash/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/gpio/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/ipc/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/lvd/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/profile/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/prot/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/scb/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/sysanalog/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/sysclk/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/sysint/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/syslib/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/syspm/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/systick/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/tcpwm/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/trigmux/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/wdt/ -IGenerated_Source\PSoC6\pdl\middleware/ -IGenerated_Source\PSoC6\pdl\middleware/em_eeprom/ -IGenerated_Source\PSoC6\pdl\utilities/ -Wa,-alh=.\CortexM0p\ARM_GCC_541\Debug/dfu_mdk_symbols.lst -g -D DEBUG -D CY_CORE_ID=0 -D CY_PSOC_CREATOR_USED=1 -D CYBLE_416045_02 -Wall -ffunction-sections -ffat-lto-objects -Og -c dfu_mdk_symbols.c -o .\CortexM0p\ARM_GCC_541\Debug\dfu_mdk_symbols.o

dfu_mdk_symbols.c:29:7: error: expected '(' before 'void'

__asm void cy_DFU_mdkAsmDummy(void)

How to solve this problem?

Thank you

EDIT: I am having an overlapping problem now

.\CortexM4\ARM_GCC_541\Debug\App1_merged.elf.tmp: Merge error: section at 0x100FFA00 from .\CortexM4\ARM_GCC_541\Debug\App0.elf overlaps section at 100FFA78 from .\CortexM4\ARM_GCC_541\Debug\App1.elf

The command 'post_build_core1.bat' failed with exit code '1'.

dfu_cm0p.Id for Both App0 and App1

    flash_app0_core0  (rx)  : ORIGIN = 0x10000000, LENGTH = 0x40000

    flash_app0_core1  (rx)  : ORIGIN = 0x10040000, LENGTH = 0x40000

    flash_app1_core0  (rx)  : ORIGIN = 0x10090000, LENGTH = 0x40000

    flash_app1_core1  (rx)  : ORIGIN = 0x100D0000, LENGTH = 0x40000

     em_eeprom         (rx)  : ORIGIN = 0x14000000, LENGTH = 0x4000

     flash_storage     (rw)  : ORIGIN = 0x100C0000, LENGTH = 0x1000

     flash_boot_meta   (rw)  : ORIGIN = 0x100FFA00, LENGTH = 0x400

dfu_cm4.Id for Both App0 and App1

    flash_app0_core0  (rx)  : ORIGIN = 0x10000000, LENGTH = 0x40000

    flash_app0_core1  (rx)  : ORIGIN = 0x10040000, LENGTH = 0x40000

    flash_app1_core0  (rx)  : ORIGIN = 0x10090000, LENGTH = 0x40000

    flash_app1_core1  (rx)  : ORIGIN = 0x100D0000, LENGTH = 0x40000

     em_eeprom         (rx)  : ORIGIN = 0x14004000, LENGTH = 0x4000

     flash_storage     (rw)  : ORIGIN = 0x100C0000, LENGTH = 0x1000

    flash_boot_meta   (rw)  : ORIGIN = 0x100FFA00, LENGTH = 0x400

The project includes BLE and EEPROM too. It was already working, but with different LENGTHs

0 Likes
3 Replies
RavikiranH_01
Employee
Employee
10 sign-ins 25 replies posted 10 replies posted

HI MuNa_4652896​,

Which compiler you are using ? .ld files will be used only for GCC. Are you using GCC ?
If you are using GCC, probably one of your application is overflowing the allocated regions. Please can you take a look ? 

Thanks

0 Likes

Sorry for the late replies.

I am using GCC Compiler. I have modified the above *.ld files as well as dfu_mdk_common.h with the following

All *.ld files

    flash_app0_core0  (rx)  : ORIGIN = 0x10000000, LENGTH = 0x10000

    flash_app0_core1  (rx)  : ORIGIN = 0x10010000, LENGTH = 0x30000

    flash_app1_core0  (rx)  : ORIGIN = 0x10040000, LENGTH = 0x20000

    flash_app1_core1  (rx)  : ORIGIN = 0x10060000, LENGTH = 0x60000

    flash_storage     (rw)  : ORIGIN = 0x100C0000, LENGTH = 0x1000

    flash_boot_meta   (rw)  : ORIGIN = 0x100FFA00, LENGTH = 0x400

    sflash_user_data  (rx)  : ORIGIN = 0x16000800, LENGTH = 0x800

    sflash_nar        (rx)  : ORIGIN = 0x16001A00, LENGTH = 0x200

    sflash_public_key (rx)  : ORIGIN = 0x16005A00, LENGTH = 0xC00

    sflash_toc_2      (rx)  : ORIGIN = 0x16007C00, LENGTH = 0x400

    efuse             (r)   : ORIGIN = 0x90700000, LENGTH = 0x100000

    ram_common        (rwx) : ORIGIN = 0x08000000, LENGTH = 0x0100

   

   

    /* note: all the ram_appX_core0 regions has to be 0x100 aligned */

    /* and the ram_appX_core1 regions has to be 0x400 aligned       */

    /* as they contain Interrupt Vector Table Remapped at the start */

    ram_app0_core0    (rwx) : ORIGIN = 0x08000100, LENGTH = 0x7F00

    ram_app0_core1    (rwx) : ORIGIN = 0x08008000, LENGTH = 0x8000

    ram_app1_core0    (rwx) : ORIGIN = 0x08000100, LENGTH = 0x7F00

    ram_app1_core1    (rwx) : ORIGIN = 0x08008000, LENGTH = 0x8000

    em_eeprom         (rx)  : ORIGIN = 0x14000000, LENGTH = 0x4000

    xip               (rx)  : ORIGIN = 0x18000000, LENGTH = 0x08000000

dfu_mdk_common.h

/* Memory region ranges per core and app */

#define CY_APP0_CORE0_FLASH_ADDR        0x10000000

#define CY_APP0_CORE0_FLASH_LENGTH      0x10000

#define CY_APP0_CORE1_FLASH_ADDR        0x10010000

#define CY_APP0_CORE1_FLASH_LENGTH      0x30000

#define CY_APP1_CORE0_FLASH_ADDR        0x10040000

#define CY_APP1_CORE0_FLASH_LENGTH      0x20000

#define CY_APP1_CORE1_FLASH_ADDR        0x10060000

#define CY_APP1_CORE1_FLASH_LENGTH      0x60000

/* DFU SDK metadata address range in Flash */

#define CY_BOOT_META_FLASH_ADDR         0x100FFA00

#define CY_BOOT_META_FLASH_LENGTH       0x200

/* Application ranges in emulated EEPROM */

#define CY_APP0_CORE0_EM_EEPROM_ADDR    0x14000000

#define CY_APP0_CORE0_EM_EEPROM_LENGTH  0x00004000

#define CY_APP0_CORE1_EM_EEPROM_ADDR    (CY_APP0_CORE0_EM_EEPROM_ADDR + CY_APP0_CORE0_EM_EEPROM_LENGTH)

#define CY_APP0_CORE1_EM_EEPROM_LENGTH  0x00004000

#define CY_APP1_CORE0_EM_EEPROM_ADDR    0x14000000

#define CY_APP1_CORE0_EM_EEPROM_LENGTH  0x00004000

#define CY_APP1_CORE1_EM_EEPROM_ADDR    (CY_APP1_CORE0_EM_EEPROM_ADDR + CY_APP1_CORE0_EM_EEPROM_LENGTH)

#define CY_APP1_CORE1_EM_EEPROM_LENGTH  0x00004000

/* Application ranges in SMIF XIP */

#define CY_APP0_CORE0_SMIF_ADDR         0x18000000

#define CY_APP0_CORE0_SMIF_LENGTH       0x00000000

#define CY_APP0_CORE1_SMIF_ADDR         (CY_APP0_CORE0_SMIF_ADDR + CY_APP0_CORE0_SMIF_LENGTH)

#define CY_APP0_CORE1_SMIF_LENGTH       0x00000000

#define CY_APP1_CORE0_SMIF_ADDR         0x14000200

#define CY_APP1_CORE0_SMIF_LENGTH       0x00000000

#define CY_APP1_CORE1_SMIF_ADDR         (CY_APP1_CORE0_SMIF_ADDR + CY_APP1_CORE0_SMIF_LENGTH)

#define CY_APP1_CORE1_SMIF_LENGTH       0x00000000

/* Application ranges in RAM */

#define CY_APP_RAM_COMMON_ADDR          0x08000000

#define CY_APP_RAM_COMMON_LENGTH        0x00000100

The application compiled successfully, but it doesn't run properly. Flashing the Bootloader App alone works well, however, when I flash the merged hex file that contains both App0 and App1. even App0 validates the Metadata step, and get stuck(like dead) while validating App1. The same happens if I decided to flash App0 only and use OTA to download the .cyacd2 for App1.

     /* Initialize dfuParams structure and DFU SDK state */

    dfuParams.timeout      = paramsTimeout;

    dfuParams.dataBuffer   = &buffer[0];

    dfuParams.packetBuffer = &packet[0];

    status = Cy_DFU_Init(&state, &dfuParams);

     /* Ensure DFU Metadata is valid */

      printf("Metadata Status = %d\r\n", status);

    status = HandleMetadata(&dfuParams);

    if (status != CY_DFU_SUCCESS)

    {

        printf("InValid Metadata\r\n");

        Cy_SysLib_Halt(0x00u);

    }

    else

    {

        printf("Valid Metadata\r\n"); //Printed

       

    }

   

    /*

    * In the case of non-software reset and user does not

    * want to stay in App0, check if there is a valid app image.

    * If there is - switch to it.

    */

    if ((Cy_SysLib_GetResetReason() != CY_SYSLIB_RESET_SOFT) && (IsButtonPressed(2000u) == false))

    {

        printf("Validating App1 now\r\n"); //Printed

        status = Cy_DFU_ValidateApp(1u, &dfuParams);

        printf("App1 Validation Status = %d \r\n", status);  //<<<< NOT Printed and nothing afterwards is done.

        if (status == CY_DFU_SUCCESS)

        {

             printf("App1 Validation Success Status = %d \r\n", status);

            /*       

            * Clear reset reason because Cy_DFU_ExecuteApp() performs       

            * a software reset.       

            * Without clearing two reset reasons would be present.       

            */

            do

            {

                Cy_SysLib_ClearResetReason();

            }while(Cy_SysLib_GetResetReason() != 0);

            /* Never returns */

            Cy_DFU_ExecuteApp(1u);

        }

        else

        {

            printf("App1 Validation Failed Status = %d \r\n", status);

        }

    }

0 Likes

Hi,

Can you please attach the complete archive of your App0 and App1?

Thanks

Ganesh

0 Likes