- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
我使用Wiced studio 6.4 编译 iperf_app , 我升级了KitProg3,
但是烧写flash报错,如下 请问如何处理?
Welcome.iperf_app-CY8CKIT_062
----------------------------------|---------|---------|
| | Static |
Module | Flash | RAM |
----------------------------------+---------+---------|
command_console | 3620 | 412 |
crc | 1060 | 0 |
DHCP_Server | 1432 | 132 |
DNS | 64 | 44 |
Host MCU-family library | 22835 | 6555 |
Interrupt Vectors | 652 | 0 |
iperf | 25242 | 2128 |
libc | 46885 | 3404 |
Networking | 3706 | 13953 |
NetX-Duo - Interfaces & Stacks | 0 | 16 |
Other | 48113 | 3461 |
Packet Buffers | 0 | 57780 |
platform | 2300 | 736 |
RAM Initialisation | 4628 | 0 |
resources | 44 | 0 |
Ring_Buffer | 156 | 0 |
SPI_Flash_Library_CY8CKIT_062 | 1172 | 352 |
Startup Stack & Link Script fill | 71 | 10 |
Supplicant - BESL | 84 | 0 |
ThreadX | 8740 | 400 |
WICED | 4404 | 1088 |
wiced_log | 300 | 1104 |
Wiced_RO_FS | 566 | 0 |
WWD | 16845 | 3197 |
----------------------------------+---------+---------|
TOTAL (bytes) | 188291 | 94772 |
----------------------------------|---------|---------|
Downloading Bootloader ...
Building apps lookup table
"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"
Downloading DCT ...
"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"
Downloading resources filesystem ... build/Welcome.iperf_app-CY8CKIT_062/filesystem.bin at sector 1 size 104...
tools/makefiles/wiced_apps.mk:335: recipe for target 'FILESYSTEM_IMAGE_DOWNLOAD' failed
make.exe[1]: *** [FILESYSTEM_IMAGE_DOWNLOAD] Error 1
Makefile:351: recipe for target 'main_app' failed
make: *** [main_app] Error 2
15:00:25 Build Finished (took 5s.381ms)
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
可以尝试按照062 WIFI-BT KIT guide 的章节3.4 Programming and Debugging in WICED中描述的步骤烧录WICED工程 - https://www.cypress.com/file/407731/download
注意烧录之前'ensure that the kit is successfully enumerated and Port Selection is set to CMSIS-DAP mode'
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
可以尝试按照062 WIFI-BT KIT guide 的章节3.4 Programming and Debugging in WICED中描述的步骤烧录WICED工程 - https://www.cypress.com/file/407731/download
注意烧录之前'ensure that the kit is successfully enumerated and Port Selection is set to CMSIS-DAP mode'