Hi Everyone.
I'm testing CY8C6247BZI-D54. I have a question about UART.
My customer want to use 9 Uart. but PSoC62 doesn't seem to support that although It have 9 x SCB blocks..
Is it right that PSoC62 doesn't use 9 uart port?
I want to know that there is possible to use.
Regards.
Robert
Solved! Go to Solution.
Robert,
You are correct, the PSoC62 has only 8 SCBs that can be configured as UARTs.
Question: Does your customer need 9 UARTs to function simultaneously?
If not, you can multiplex the input/output of one or more SCBs as long as the UART ports being multiplexed are not operating simultaneously.
Additionally the USB-FS is commonly used as a UART interface if the host device can be configured as a "COM" device.
Len
Robert,
You are correct, the PSoC62 has only 8 SCBs that can be configured as UARTs.
Question: Does your customer need 9 UARTs to function simultaneously?
If not, you can multiplex the input/output of one or more SCBs as long as the UART ports being multiplexed are not operating simultaneously.
Additionally the USB-FS is commonly used as a UART interface if the host device can be configured as a "COM" device.
Len