- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
thanks your supports.
My name is david yu.
I sent a e-mail with the same subject in 2 July.
your reply is very helpful for me.
I also a little question about it.
1. the reflashing speed.
- I compared the two demon software, CE223726 in PSoC creator and emWin_TFT_FreeRTOS in ModusToolbox.
when changing the image, PSoc creator is faster than modustoolbox.
why PSoc creator is fast? I guess this because of RTOS .
Can I speed up the speed changing a image in RTOS?
2. the moving image
- I am trying to show the movie file in tft LCD using the enWinGraphic example file.
but i couldn't do it.
would you tell me the example source code?
thanks
i copy the previous e-mail in below
--------------------------------
Hi.
I am an engineer in Seoul, South Korea.
I got an PSoC6 Wifi BT Pioneer Kit with the TFT LCD 2.4 inch.
I am trying to work to show the sypress log using the example source code of the CE225248_DisplayBuffer.
But I cannot.
Would you give me the information for this?
also can you give me the source of the sypress log showing in the TFT LCD?
I use the PSoC creater 4.4 version.
thanks
My E-mail : yugh@techrein.com
Solved! Go to Solution.
- Labels:
-
PSoC 6 MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The reason why the PSoC Creator project is faster is because it uses a driver implemented in UDBs (our programmable digital blocks).
While the ModusToolbox project uses a bit bang method to drive the TFT, which is much slower. Currently, we don't support UDBs with ModusToolbox.