- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
For PSoC 62 do I need have always two project with two main.c ?
The resulting code is one hex file?
(I'm using PSoC creator)
Solved! Go to Solution.
- Labels:
-
PSoC 6 MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @jsmith678x,
I am not sure I understood your question.
When you create an empty PSoC 62 project in PSoC Creator, it creates one project with 2 main.c files, one for CM0+ and one more for CM4 CPU. You can choose not to use the main_cm0p.c and run your application on the CM4 CPU. In that case, the CM0+ CPU just enables the CM4 CPU.
The resulting code is one hex file?
Yes, this is correct. You can program the device using the hex file in the Project.cydsn\CortexM4\ARM_GCC_541\Debug directory.
Rakshith M B
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @jsmith678x,
I am not sure I understood your question.
When you create an empty PSoC 62 project in PSoC Creator, it creates one project with 2 main.c files, one for CM0+ and one more for CM4 CPU. You can choose not to use the main_cm0p.c and run your application on the CM4 CPU. In that case, the CM0+ CPU just enables the CM4 CPU.
The resulting code is one hex file?
Yes, this is correct. You can program the device using the hex file in the Project.cydsn\CortexM4\ARM_GCC_541\Debug directory.
Rakshith M B