Hi,
as long as there is no Silicon available, i would like to start some ideas in the PSoC-Creator. I want to be ready at the time, the first samples are available for me.
I use the actual "PSoC Creator 4.0 Update 1 (4.0.0.432)". Is there an addon to implement the features of the PSoC6? Or, ist there anything I'm overlooking?
...hoping to start my first PSoC6 Project.....
Best regards,
Martin Kraus
Solved! Go to Solution.
Hi Martin!
You aren't missing anything. At the moment support for PSoC 6 is not enabled in PSoC Creator, and the PDL is not available. So for the time being, from a customer perspective, software development is still "theoretical."
From a practical point of view, while moving right along, the entire firmware development process and PDL is a moving target.