Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 6 Forum Discussions

baga_4725781
Level 3
Level 3
First like received First like given

I'm using a PSoC 6 WiFi-BT Prototyping Kit

I followed the sequence (forgot the document it's in)

Board Setup

  1. Use the USB lead to connect your Mbed to a PC. The status light will come on, indicating it has power.
  2. Check if kit is in CMSIS-DAP mode LED1 (POWER) and LED2 (STATUS) as shown in the image below, LED2 can be blinking or solid.
  3. Download the fw-loader from Cypress Semiconductor Github.
  4. Execute the following command in command line, fw-loader.exe --update-kp3. If the connected kit is not detected after executing this command, please enter into bootloader mode by holding down the "Mode Select" button (SW3) before plugging in the board. Then run the fw-loader.exe again.
  5. After command is executed successfully please press the SW3 Mode button for 3 seconds and release.
  6. Kit should now be connected in DAPLink mode as shown in the image below (LED1 should glow).

The update seemed to work (eg no obvious failures).
However, this sequence is supposed to make the device look like a drive (eg D:). It does not. Is this a depreciated feature, known bug, or what? It seems a previous use was to download your executable on the "drive" in order to program the device.
Mainly a curiosity question.
Thanks! ... bandit
0 Likes
1 Solution
NoriakiT_91
Employee
Employee
100 likes received 50 likes received 25 likes received

If you find a mass-storage drive like 😧 the KitProg3 is recognized as an mbed Composite Device.  Please confirm the device manager selecting the menu item "View>Devices by connection".

GS004795.png

In this mode, the STATUS LED blinks fast (2Hz) and the Modus Toolbox failed to find a CMSIS-DAP device.

GS004796.png

Please push the MODE switch once to change the mode to KitProg3 CMSIS-DAP.

GS004797.png

In this mode, the STATUS LED stops blinking and turns on stably.

Regards,

Noriaki

View solution in original post

0 Likes
1 Reply
NoriakiT_91
Employee
Employee
100 likes received 50 likes received 25 likes received

If you find a mass-storage drive like 😧 the KitProg3 is recognized as an mbed Composite Device.  Please confirm the device manager selecting the menu item "View>Devices by connection".

GS004795.png

In this mode, the STATUS LED blinks fast (2Hz) and the Modus Toolbox failed to find a CMSIS-DAP device.

GS004796.png

Please push the MODE switch once to change the mode to KitProg3 CMSIS-DAP.

GS004797.png

In this mode, the STATUS LED stops blinking and turns on stably.

Regards,

Noriaki

0 Likes