Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 6 Forum Discussions

Anonymous
Not applicable

Hello PSoC MCU Developers!

I'm pleased to announce the release of a brand new PSoC 6 kit, the PSoC 6 WiFi-BT Pioneer Kit CY8CKIT-062-WiFi-BT.

The PSoC® 6 WiFi-BT Pioneer Kit (CY8CKIT-062-WiFi-BT) is a low-cost hardware platform that enables design and prototyping of the PSoC 62 MCU and the Murata LBEE5KL1DX Module (CYW4343W WiFi + Bluetooth Combo Chip).. The kit includes the CY8C6247 device, a Murata LBEE5KL1DX Module (WiFi/BT combo chip on-board) 512-Mb Quad-SPI NOR flash, on-board programmer/debugger (Kitprog2), EZ-PD™ CCG3 Type-C MCU, CapSense touch slider, buttons, and proximity sensor, and is Arduino Uno compatible. It also comes with a TFT Display shield board (CY8CKIT-028-TFT) with on-board PDM-PCM microphone, motion sensor, light sensor, and audio jack. The TFT Display shield board will be orderable separately from the kit as well.

SS2_2613.jpg

With this kit, you can develop standalone PSoC 6 MCU designs, or you can create PSoC 6 + WiFi designs. For standalone PSoC 6 MCU designs, PSoC Creator is the recommended design environment. For PSoC 6 + WiFi designs, WICED Studios 6.1 is the recommended design environment.

Feel free to leave your comments, questions or feedback, we appreciate it!

5 Replies
Anonymous
Not applicable

Wow! Looks awesome!

Any future giveaway for this?

0 Likes
Anonymous
Not applicable

Is that the same WiFi+BT chip that's on the new Raspberry Pi 3 Model B+?

0 Likes

Hi Eric

The 062 kit has a CYW4343W which is an almost identical chip to the CYW43438 which is on the Pi Zero W and the original Pi3.

The Pi3 B+ has a CYW43455 chip.

The main difference is the CYW43455 supports 802.11ac and 2.4/5GHz whereas the CYW43438/W is 802.11n 2.4GHz only.

Hope that helps.

Thanks

Graham

Helpful~

0 Likes
ravo
Level 5
Level 5
5 solutions authored 100 replies posted 250 sign-ins

Nice info, when full datasheet for PSoC 62 - CY8C6247BZI-D54 will be available ?

Regards Radim

0 Likes