Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
AnCi_2234676
Level 4
Level 4
10 replies posted 5 replies posted 10 questions asked

I need to generate a buffer filled with random bytes not equal to 0 and I was wondering what would be the most effective in terms of power consumption.

First, between the PRNG and the TRNG, is there a significant difference in power consumption?

Also, out of the following options, which one would be the best in terms of power consumption:

  1. Generate a 4 bytes random number, but only check the first byte. If it is not 0, add it to the buffer. Repeat until buffer is full.
  2. Generate a 4 bytes random number. Add the 4 bytes to the buffer if none of them is 0. Repeat until buffer is full.
  3. Generate a 4 bytes random number. Loop through the 4 bytes. If it is not 0, add it to the buffer. Repeat until buffer is full.

Thanks!

0 Likes
1 Solution
Hari
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi AnCi_2234676

PRNG would be lower power consuming since it is implemented using a LFSR. The TRNG has 6 ring oscillators running between 90 and above 500 MHz.

As far as the most efficient way to store non-zero 32-bit numbers, just check the entire 32-bit value for zero once you get it.

Regards

Hari

View solution in original post

0 Likes
1 Reply
Hari
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi AnCi_2234676

PRNG would be lower power consuming since it is implemented using a LFSR. The TRNG has 6 ring oscillators running between 90 and above 500 MHz.

As far as the most efficient way to store non-zero 32-bit numbers, just check the entire 32-bit value for zero once you get it.

Regards

Hari

0 Likes