- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I like to access a SPI slave with 3-wire SPI implementation on PSOC6.
The component SPI(SCB v2.0) doesn't seem to have a 3 wire SPI implementation/sub-mode.
I do see National Semiconductor (microwire), but this is still 4 wire.
Any there a way to support this in PSOC6?
I see that this is supported in other PSOC family.
Thanks!
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Another solution if you use an SPI on Port 8 or 9 would be to use SmartIO and the internal Data Unit to route the data automatically to MOSI and MISO. The Data Unit has to be configured as counter that controls the multiplexing of the data via the LUTs. Chip Select should be used to reset the Data Unit.
Third solution and most complex would be a custom component using the UDBs. But this is also the most flexible in case the SPI communication has some special timing requirements.
Kind Regards,
Achim