- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I recently started having problems with my PSoC 6 Pioneer kit (CY8CKIT-062-BLE). I have been using it successfully since September 2019. Since before yesterday, when I click on the program button, the Select debug target window appears, I am able to see my KitProg 3, but the 2 options I used to be able to choose (Cortex M4 and M0+) are just gone, they do not appear anymore, so I cannot program my kit anymore.
I am using CYC6347BZI-BLD53 (Y w/ gestures) in the device selector. I tested on both the computers I have been using in the past month and none work. I am sure it a question of programming mode of the device, or firmware or driver. I just didn't find a post addressing this family of devices yet. I have read pressing the reset button 10s could help but it didn't work for me. I also made sure there was no other program using the kit when plugged in, as this seemed to be one common problem with this issue. I went to PSoC programmer app and the device was properly recognized and connected. I clicked on upgrade firmware and it worked, but still no use. After a full day of programming, I had 2 instances of usb device not recognized or malfunctioned when replugging the kit to my PC. Those 2 happened like in the last 10 tries I have made. The kit is still recognized most of the time but this worried me quite a bit.
Could it be a hardware problem?? I hope not, it would be very surprising as I am not carrying the kit around. I am sure there is a way to change the programming mode or whatnot of this device? thanks!
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
FYI, I took pictures of my board running attached hex programmed using PSoC Programmer.
I'm seeing LED2 and LED4 light orange-yellow, LED3 in Green.
And also LED5 is blinking Green.
SW5 Middle Position (3.3V)
SW7 Right Position
SW6 Right Position
J8 Short
moto
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
There could be many reasons which cause the symptom you described.
In the worst case the device on your board could have been damaged.
You wrote that you have already tried the mode switch.
And you wrote that you have tried to update the firmware.
Here, I wonder which version of "PSoC Programmer" you are using.
I think that currently the newest is 3.28.6.
If yours is older, please download and update to the newest one.
We can download PSoC programmer from
https://www.cypress.com/documentation/software-and-drivers/psoc-programmer-archive
Please select the newest and try it.
moto
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
Hi, thank you for mentioning the position of your switches. My problem is solved: I had SW6 facing left.. SW6 is target select on the schematic. Afterwards I was able to upload your hex file. I just never thought of switches. PSoC creator works too. Thank you so much!