- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I am developing a low-power application using CY8CKIT-062-BLE board.
I followed the application note "PSoC 6 MCU Device Firmware Update Software Development Kit Guide" and configured a "map A" BLE DFU Memory Maps.
On the basis of above configuration, I am trying to use the non-volatile memory of PSoC by following the example code : CE220120
So, In the App1, I declare a const value before the "main()" function:
CY_ALIGN(CY_FLASH_SIZEOF_ROW)
const uint8_t flashData[CY_FLASH_SIZEOF_ROW] = {0}; /* The array will be placed in Flash */
Then in the the "main()" function, I write the following code:
uint8_t ramData[CY_FLASH_SIZEOF_ROW];
Initial_finished=false;
/* Initialize the data in RAM that will be written into flash */
for(uint16_t index = 0; index < CY_FLASH_SIZEOF_ROW; index++)
{
ramData[index] = (uint8_t)index;
}
cy_en_flashdrv_status_t flashWriteStatus;
flashWriteStatus = Cy_Flash_WriteRow((uint32_t)(flashData), (const uint32_t *)ramData);
The App1 properly works after updating the App0 to App1.
However, after I powered off the board and powered on again (or put RESET button ), the system cannot execute App1 properly; it keeps in App0 and waiting for updating image.
I called printf to check what is wrong, and found after resetting, in App0 "status = Cy_DFU_ValidateApp(1u, &dfuParams)", the status is not "CY_DFU_SUCCESS".
If I remove the "Cy_Flash_WriteRow()" function in App1, the App1 can be normally executed after resetting the system.
So my question is:
1. What makes "Cy_DFU_ValidateApp(1u, &dfuParams)" failed after calling "Cy_Flash_WriteRow()" in App1?
2. How to make sure "Cy_DFU_ValidateApp(1u, &dfuParams)" not failed after calling "Cy_Flash_WriteRow()" in App1?
Thank you very much for your kind help!!
Best regards,
Jiabin
Solved! Go to Solution.
- Labels:
-
PSoC 6 MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
App0 verifies App1 (uses CRC if you are using the Infineon released Code Example as it is) before jummpig to it.
From the above explanation, it looks like App0 FAILED to VERIFY App1.
During the build process (on host PC) a CRC generated and attached to the App1 firmware. It is placed in ".cy_app_signature" section. Please see your App1 main.c & Linker files for details.
Cy_Flash_WriteRow() called from App1 seems to be modifying the "flash" content that is used for CRC calculation; and hence CRC is doesn't match after calling Cy_Flash_WriteRow().
When you do Cy_Flash_WriteRow(); you could modify the App1 to write to a region outside the application flash area. For example, you can write to emEeprom region or any other flash region outside the App1's scope.
See https://github.com/Infineon/mtb-example-psoc6-dfu-basic/blob/master/bootloader_cm4/source/dfu_user.c for emeeprom address range and its usage on P6
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
App0 verifies App1 (uses CRC if you are using the Infineon released Code Example as it is) before jummpig to it.
From the above explanation, it looks like App0 FAILED to VERIFY App1.
During the build process (on host PC) a CRC generated and attached to the App1 firmware. It is placed in ".cy_app_signature" section. Please see your App1 main.c & Linker files for details.
Cy_Flash_WriteRow() called from App1 seems to be modifying the "flash" content that is used for CRC calculation; and hence CRC is doesn't match after calling Cy_Flash_WriteRow().
When you do Cy_Flash_WriteRow(); you could modify the App1 to write to a region outside the application flash area. For example, you can write to emEeprom region or any other flash region outside the App1's scope.
See https://github.com/Infineon/mtb-example-psoc6-dfu-basic/blob/master/bootloader_cm4/source/dfu_user.c for emeeprom address range and its usage on P6
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content