Hi,
你可能没有预先安装离线包,也需要设置一些系统变量来更好使用offline模式。
关于设置offline模式的全部信息,请参考:
https://community.infineon.com/t5/Resource-Library/Use-Offline-Content-in-Eclipse-IDE-for-ModusToolb...
Best regards
使用的 offline模式,
Summary:
BSP: CY8CKIT-062-BLE
Template Application(s): Dual-CPU Empty PSoC6 App, Dual-CPU IPC Pipes
Note: The 'Dual-CPU Empty PSoC6 App, Dual-CPU IPC Pipes' application template(s) use(s) the ModusToolbox 2.x format. The application(s) do(es) not support 3.x features. See KBA236134 for instructions on how to migrate the application(s) for 3.x content compatibility.
Application(s) Root Path: D:/mymdsToolsw
Press "Create" to create the selected application(s).
Collecting application data...
Info: The following entered on the command line will create the exact same project as that created with the GUI tool:
D:/Infineon/Tools/ModusToolbox/tools_3.0/project-creator/project-creator-cli.exe --board-id CY8CKIT-062-BLE --board-uri https://github.com/cypresssemiconductorco/TARGET_CY8CKIT-062-BLE --board-commit latest-v2.X --app-id mtb-example-psoc6-dual-cpu-empty-app --app-uri https://github.com/cypresssemiconductorco/mtb-example-psoc6-dual-cpu-empty-app --app-commit latest-v2.X --cypress-tools D:/Infineon/Tools/ModusToolbox/tools_3.0 --target-dir D:/mymdsToolsw --user-app-name Dual-CPU_Empty_PSoC6_App --use-modus-shell --offline
Starting application creation for 'D:/mymdsToolsw/Dual-CPU_Empty_PSoC6_App'.
Acquiring the application source 'https://github.com/cypresssemiconductorco/mtb-example-psoc6-dual-cpu-empty-app'.
Acquired application source successfully.
Loading the application.
Application load failed.
ERROR:Application creation failed.
ERROR:the directory 'D:/mymdsToolsw/Dual-CPU_Empty_PSoC6_App' does not contain the file 'Makefile'
Skipping export of the "Dual-CPU_Empty_PSoC6_App" application to Eclipse IDE for ModusToolbox™.
Info: The following entered on the command line will create the exact same project as that created with the GUI tool:
D:/Infineon/Tools/ModusToolbox/tools_3.0/project-creator/project-creator-cli.exe --board-id CY8CKIT-062-BLE --board-uri https://github.com/cypresssemiconductorco/TARGET_CY8CKIT-062-BLE --board-commit latest-v2.X --app-id mtb-example-psoc6-dual-cpu-ipc-pipes --app-uri https://github.com/cypresssemiconductorco/mtb-example-psoc6-dual-cpu-ipc-pipes --app-commit latest-v2.X --cypress-tools D:/Infineon/Tools/ModusToolbox/tools_3.0 --target-dir D:/mymdsToolsw --user-app-name Dual-CPU_IPC_Pipes --use-modus-shell --offline
Starting application creation for 'D:/mymdsToolsw/Dual-CPU_IPC_Pipes'.
Acquiring the application source 'https://github.com/cypresssemiconductorco/mtb-example-psoc6-dual-cpu-ipc-pipes'.
Acquired application source successfully.
Loading the application.
Application load failed.
ERROR:Application creation failed.
ERROR:the directory 'D:/mymdsToolsw/Dual-CPU_IPC_Pipes' does not contain the file 'Makefile'
Skipping export of the "Dual-CPU_IPC_Pipes" application to Eclipse IDE for ModusToolbox™.
4 error(s), 0 warning(s)
Summary:
ERROR:Failed to create and export "Dual-CPU_Empty_PSoC6_App" application.
ERROR:Failed to create and export "Dual-CPU_IPC_Pipes" application.
您好还有个问题,我目前使用的是 offline模式,但是在这儿要等一会儿,能否设置一下,直接使用 offline模式以节约时间,谢谢
Hi,
你可能没有预先安装离线包,也需要设置一些系统变量来更好使用offline模式。
关于设置offline模式的全部信息,请参考:
https://community.infineon.com/t5/Resource-Library/Use-Offline-Content-in-Eclipse-IDE-for-ModusToolb...
Best regards
您好,无法更改 MCU 型号呀,之前是通过https://community.infineon.com/t5/PSoC-Creator-Designer/PSoC-6-MCU-CY8C61x5-support-in-PSoC-Creator/... 更改 MCU 型号
现在 是最新的 modustoolbox-offline-content-20221027.zip,更改芯片型号
是这个报警
Loading the ModusToolbox Technology Packs and Early Access Packs
Finished loading the ModusToolbox Technology Packs and Early Access Packs (6 ms)
Loading the tools information
Finished loading the tools information (38 ms)
Loading the manifest data
Using the executable path for the tools directory.
WARNING:Error downloading 'https://modustoolbox.infineon.com/manifests/mtb-super-manifest/v2.X/mtb-super-manifest-fv2.xml' -- Host raw.githubusercontent.com not found
ERROR:all super manifests were invalid, no data loaded
ERROR:Manifest loading completed with erro
我的modustoolbox是 3.0版本
你可以试试添加CyRemoteManifestOverride这个变量,应该可以解决BSP assistant的manifest问题:
https://community.infineon.com/t5/Knowledge-Base-Articles/Offloading-the-Manifest-Files-of-ModusTool...
Dear Manager
使用Modustool 开发,如果只用M4,是不是也要创建个工程把M0给休眠以降低功耗,Thanks
Hi:
1、如果你使用的是双核POC6芯片,那么M4的启动必须是要通过M0来启动的。
2、如果你启动了M4不再需要M0,你可以将M0低功耗运行,在code example中可以作为参考。
3、最好一次只讨论一个话题,如果还有其他问题可以再创建一个新的,尽量不要在一个问题下面讨论多个其他方向的话题。
谢谢