公告

大中华汽车电子生态圈社区并入开发者社区- 更多资讯点击此

Tip / 登入 to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
1313_3839421
Level 3
Level 3
10 replies posted 10 questions asked 5 replies posted

Miniprog3 烧录器PC端毫无征兆的突然枚举失败, 烧录器指示灯也不亮了,这种现象一般是什么原因导致的?

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

0 点赞
1 解答
Vison_Zhang
Moderator
Moderator
Moderator
First comment on KBA 750 replies posted 250 sign-ins

看样子是坏了。

在原帖中查看解决方案

0 点赞
7 回复数
LinglingG_46
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 10 questions asked

1: 用万用表量一下VDD和GND之间的阻抗。

2:看一下你的programmer,是不是最新的:http://www.cypress.com/?rID=38050&source=header

3: 根据下面链接重新安装一下minprog3的驱动:Binding miniprog3 to the appropriate driver man... | Cypress Developer Community

0 点赞

你好,首先非常感谢您的答复,

1:VDD和GND之间的阻抗为50KΩ

2:我目前在用的programmer版本为3.29.0是最新的

3:链接下的MiniProgUpdateDriver.pdf官网和论坛都没有找到,该文件的下载链接方便提供一下吗

再次感谢!

0 点赞
LinglingG_46
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 10 questions asked

未知USB驱动这个地方,鼠标右击,然后选择到minprog3的驱动模式。

The mprog3.inf file located at the following address is the driver file which need to be binded with miniprog3. This inf file points to sys file which is required for connecting miniprog3 to USB.

C:\Program Files\Cypress\Programmer\3.12\drivers\mprog3

重新安装USB的驱动。

0 点赞

你好 ,更新驱动之后依旧无法使用,MiniProg3的指示灯也不亮,是不是硬件上出问题了,刚买的还不到一个月。

pastedImage_0.png

0 点赞
Vison_Zhang
Moderator
Moderator
Moderator
First comment on KBA 750 replies posted 250 sign-ins

重启一下电脑试试,也换台电脑试试(测试电脑必须安装 PSoC Programmer),从测量的参数来看,不像是坏了。设备有发烫现象吗?

0 点赞

换了三台电脑都是枚举出问题(都安装了PSoC Programmer  3.29.0),设备没有发烫过,不像是短路烧坏了。换另外一个好的MiniProg3不管是第一次安装还是更新驱动都没问题一切正常。所以异常的这个烧录器是不是硬件上有问题。

0 点赞
Vison_Zhang
Moderator
Moderator
Moderator
First comment on KBA 750 replies posted 250 sign-ins

看样子是坏了。

0 点赞