Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
pagansjb
Level 2
Level 2
First like given 10 replies posted First like received

When I followed the descriptions for 'Secure Blinky LED FreeRTOS' example with CYB06445LQI-S3D42,

I faced error messages with 'cysecuretools --target cyb06xx7 --policy ./policy/policy_single_CM0_CM4.json provision-device' as like the below.


2022-06-09 17:10:59,351 : C : INFO : ######################################################################
2022-06-09 17:10:59,351 : C : INFO : Provisioning packet is created
2022-06-09 17:10:59,351 : C : INFO : ######################################################################
2022-06-09 17:10:59,355 : C : INFO : Target: cyb06xx7
2022-06-09 17:10:59,369 : P : INFO : Target type is cy8c64xx_cm4_full_flash
2022-06-09 17:10:59,377 : P : INFO : DP IDR = 0x6ba02477 (v2 rev6)
2022-06-09 17:10:59,378 : P : INFO : AHB-AP#0 IDR = 0x84770001 (AHB-AP var0 rev8)
2022-06-09 17:10:59,381 : P : INFO : AHB-AP#2 IDR = 0x24770011 (AHB-AP var1 rev2)
2022-06-09 17:10:59,386 : P : INFO : AHB-AP#0 Class 0x1 ROM table #0 @ 0xf1000000 (designer=034 part=105)
2022-06-09 17:10:59,390 : P : INFO : AHB-AP#2 Class 0x1 ROM table #0 @ 0xe00ff000 (designer=034 part=105)
2022-06-09 17:10:59,392 : P : INFO : [0]<e0080000:CTI class=9 designer=43b part=906 devtype=14 archid=0000 devid=40800:0:0>
2022-06-09 17:10:59,394 : P : INFO : [3]<e008e000:TPIU M3 class=9 designer=43b part=923 devtype=11 archid=0000 devid=ca1:0:0>
2022-06-09 17:10:59,395 : P : INFO : [4]<e007f000:ROM class=1 designer=034 part=105>
2022-06-09 17:10:59,395 : P : INFO : AHB-AP#2 Class 0x1 ROM table #1 @ 0xe007f000 (designer=034 part=105)
2022-06-09 17:10:59,398 : P : INFO : [0]<e000e000:SCS v7-M class=14 designer=43b part=00c>
2022-06-09 17:10:59,400 : P : INFO : [1]<e0001000:DWT v7-M class=14 designer=43b part=002>
2022-06-09 17:10:59,401 : P : INFO : [2]<e0002000:FPB v7-M class=14 designer=43b part=003>
2022-06-09 17:10:59,403 : P : INFO : [3]<e0000000:ITM v7-M class=14 designer=43b part=001>
2022-06-09 17:10:59,404 : P : INFO : [4]<e0042000:CTI class=9 designer=43b part=906 devtype=14 archid=0000 devid=40800:0:0>
2022-06-09 17:10:59,406 : P : INFO : [5]<e0041000:ETM M4 class=9 designer=43b part=925 devtype=13 archid=0000 devid=0:0:0>
2022-06-09 17:10:59,407 : P : INFO : CPU core #1 is Cortex-M4 r0p1
2022-06-09 17:10:59,409 : P : INFO : FPU present: FPv4-SP-D16-M
2022-06-09 17:10:59,411 : P : INFO : 4 hardware watchpoints
2022-06-09 17:10:59,412 : P : INFO : 6 hardware breakpoints, 4 literal comparators
2022-06-09 17:10:59,415 : C : INFO : Use system AP
2022-06-09 17:10:59,420 : P : INFO : Clearing TEST_MODE bit...
2022-06-09 17:10:59,420 : C : INFO : Probe ID: 190C13010a0e161b030a0e1600000000000000002e127069
2022-06-09 17:10:59,422 : C : INFO : Secure Flash Boot version: 4.0.2.1842
2022-06-09 17:10:59,422 : C : ERROR : Memory transfer fault @ 0x40230040-0x40230043. Check the log for details
Error: Failed processing!


How can I resolve this issue?

0 Likes
1 Solution
AlenAn14
Moderator
Moderator
Moderator
500 replies posted 100 solutions authored 250 replies posted

Hi @pagansjb ,

I believe you are using the wrong command.

The target device you are using is CYB06445LQI-S3D42 which is cyb06xx5 device and not cyb06xx7 device.

Can you please try changing the command to the following :

'cysecuretools --target cyb06xx5 --policy ./policy/policy_single_CM0_CM4.json provision-device'

Warm Regards
Alen

View solution in original post

0 Likes
3 Replies
AlenAn14
Moderator
Moderator
Moderator
500 replies posted 100 solutions authored 250 replies posted

Hi @pagansjb ,

I believe you are using the wrong command.

The target device you are using is CYB06445LQI-S3D42 which is cyb06xx5 device and not cyb06xx7 device.

Can you please try changing the command to the following :

'cysecuretools --target cyb06xx5 --policy ./policy/policy_single_CM0_CM4.json provision-device'

Warm Regards
Alen

0 Likes

Thanks, as you mentioned, I've used wrong command.

0 Likes
AlenAn14
Moderator
Moderator
Moderator
500 replies posted 100 solutions authored 250 replies posted

Hi @pagansjb ,

Glad your query is resolved!

Please feel free to post any queries or issues you may have on Infineon products in the community and we will be happy to help

Thanks and Regards,
Alen
Cypress Semiconductor Corporation
An Infineon Technologies Company

0 Likes