- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
we are working on the Smart Lock project using the Matter protocol or CHIP
I am trying to connect the PSOC 6 with matter protocol/ CHIP software loaded and the Raspberry pi wifi/zigbee interface
not connecting
Matter protocol buildwithmatter.com
i followed the docs provided in the /connectedhomeip/examples/lock-app/P6/Readme.md
I executed the : zcl OnOff On 1234 1 0 ---- command
not connecting , below is the error message
Please reply me the possible solution.
----------------------------------------------------------------------------------------------------------------------------------------------------------
chip-device-ctrl > zcl OnOff On 1234 1 0
[1637573653.279080][9954:9960] CHIP:DL: Avahi resolve failed
[1637573653.279196][9954:9960] CHIP:DIS: Node ID resolved failed with ../../src/platform/Linux/DnssdImpl.cpp:692: CHIP Error 0x000000AC: Internal error
[1637573653.279257][9954:9960] CHIP:CTL: Error resolving node id: ../../src/platform/Linux/DnssdImpl.cpp:692: CHIP Error 0x000000AC: Internal error
Failed to update node address: 172
^Z[1637574457.431856][9954:9954] CHIP:DL: writing settings to file (/tmp/chip_counters.ini-zQ6w1Q)
[1637574457.433052][9954:9954] CHIP:DL: renamed tmp file to file (/tmp/chip_counters.ini)
[1637574457.433175][9954:9954] CHIP:DL: NVS set: chip-counters/boot-reason = 5 (0x5)
[1637574457.433553][9954:9954] CHIP:DL: writing settings to file (/tmp/chip_counters.ini-mnlqAQ)
[1637574457.434501][9954:9954] CHIP:DL: renamed tmp file to file (/tmp/chip_counters.ini)
[1637574457.434610][9954:9954] CHIP:DL: NVS set: chip-counters/total-operational-hours = 0 (0x0)
[1637574457.434666][9954:9954] CHIP:DL: Inet Layer shutdown
[1637574457.434892][9954:9954] CHIP:DL: BLE shutdown
[1637574457.434957][9954:9954] CHIP:DL: System Layer shutdown
pure virtual method called
terminate called without an active exception
Aborted (core dumped)
(python_env) ubuntu@ubun
- Labels:
-
ispn:39620:1:0
-
l1:314:1:0
-
PSoC6MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Are you having issues in interfacing the PSoC with the RPi or are you having issues when you try to connect to WiFI AP?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Murali,
I am having issue while sending commands from the command prompt from Raspberry pi to PSOC6 -43012 controller.
docs: buildwithmatter.com
I am using the PSOC6 for smartlock
i am using the raspberry pi to send the commands to psoc6 using the wifi
i mean switching led off in the psoc6 board which is used for the smart lock using the command from the raspberry pi <zcl OnOff On 1234 1 0>
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello
How are the commands being sent from the RPI? Is it through some wired connection between the RPI and the PSoC or is it using the WiFi interface?
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
It is through wifi
reference: buildwithmatter.com
https://github.com/project-chip/connectedhomeip#readme
we are using example: connectedhomeip/example/lock-app/p6
we are following the readme.rd file in the P6 example code.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Do you have a way for me to reproduce this and debug? This is new for me too and would probably need to understand what is happening before giving out a solution.