- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
we are working on the Smart Lock project using the Matter protocol or CHIP
I am trying to connect the PSOC 6 with matter protocol/ CHIP software loaded and the Raspberry pi wifi/zigbee interface
not connecting
Matter protocol buildwithmatter.com
i followed the docs provided in the /connectedhomeip/examples/lock-app/P6/Readme.md
I executed the : zcl OnOff On 1234 1 0 ---- command
not connecting , below is the error message
Please reply me the possible solution.
----------------------------------------------------------------------------------------------------------------------------------------------------------
chip-device-ctrl > zcl OnOff On 1234 1 0
[1637573653.279080][9954:9960] CHIP:DL: Avahi resolve failed
[1637573653.279196][9954:9960] CHIP:DIS: Node ID resolved failed with ../../src/platform/Linux/DnssdImpl.cpp:692: CHIP Error 0x000000AC: Internal error
[1637573653.279257][9954:9960] CHIP:CTL: Error resolving node id: ../../src/platform/Linux/DnssdImpl.cpp:692: CHIP Error 0x000000AC: Internal error
Failed to update node address: 172
^Z[1637574457.431856][9954:9954] CHIP:DL: writing settings to file (/tmp/chip_counters.ini-zQ6w1Q)
[1637574457.433052][9954:9954] CHIP:DL: renamed tmp file to file (/tmp/chip_counters.ini)
[1637574457.433175][9954:9954] CHIP:DL: NVS set: chip-counters/boot-reason = 5 (0x5)
[1637574457.433553][9954:9954] CHIP:DL: writing settings to file (/tmp/chip_counters.ini-mnlqAQ)
[1637574457.434501][9954:9954] CHIP:DL: renamed tmp file to file (/tmp/chip_counters.ini)
[1637574457.434610][9954:9954] CHIP:DL: NVS set: chip-counters/total-operational-hours = 0 (0x0)
[1637574457.434666][9954:9954] CHIP:DL: Inet Layer shutdown
[1637574457.434892][9954:9954] CHIP:DL: BLE shutdown
[1637574457.434957][9954:9954] CHIP:DL: System Layer shutdown
pure virtual method called
terminate called without an active exception
Aborted (core dumped)
(python_env) ubuntu@ubun
- Labels:
-
PSoC 6 MCU