- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I was using HAL PWM code to set the PWM resource to 100% dutycycle. What I got is that at 100% dutycycle, the PWM turned OFF (effectively 0%).
The issue is actually in the function cyhal_pwm_set_period_and_compare().
This is because:
cyhal_pwm_set_duty_cycle(&obj, 100, frequencyhal_hz)
{
...
uint32_t period = obj->clock_hz / frequencyhal_hz;
uint32_t width = (uint32_t)(100 * 0.01f * period);
cyhal_pwm_set_period_and_compare(obj, period, width); /* Here period = width @ 100% dc */
{
...
Cy_TCPWM_PWM_SetPeriod0(obj->base, obj->resource.channel_num, period - 1u); /* The period count is corrected here */
...
else
{
Cy_TCPWM_PWM_SetCompare0(obj->base, obj->resource.channel_num, compare);
/* Although the period was corrected (period-1) the compare in this case is period + 1. The compare count was not corrected. */
/* When compare > period, the result is an effective 0% dc */}
May I recommend the following changes to function cyhal_pwm_set_period_and_compare():
static cy_rslt_t cyhal_pwm_set_period_and_compare(cyhal_pwm_t *obj, uint32_t period, uint32_t compare)
{
if (period < 1 || period > (uint32_t)((1 << CYHAL_TCPWM_DATA[obj->resource.block_num].max_count)) - 1)
return CYHAL_PWM_RSLT_BAD_ARGUMENT;
period = period - 1u; /* Make the period count correction here. */
/* This fixes the issue where period == compare (ie duty_cycle == 100 percent) */
if (compare > period)
compare = period;
cyhal_gpio_t pin = obj->pin;
cyhal_gpio_t pin_compl = obj->pin_compl;
Cy_TCPWM_PWM_SetCompare0(obj->base, obj->resource.channel_num, 0u);
Cy_TCPWM_PWM_SetPeriod0(obj->base, obj->resource.channel_num, period);
bool swapped_pins = (CY_UTILS_GET_RESOURCE(pin, cyhal_pin_map_tcpwm_line_compl) != NULL) && (CY_UTILS_GET_RESOURCE(pin_compl, cyhal_pin_map_tcpwm_line) != NULL);
bool is_center_aligned = (TCPWM_CNT_TR_CTRL2(obj->base, obj->resource.channel_num) == CY_TCPWM_PWM_MODE_CNTR_OR_ASYMM) ||
(TCPWM_CNT_TR_CTRL2(obj->base, obj->resource.channel_num) == CY_TCPWM_PWM_MODE_CNTR_OR_ASYMM_UO_SWAPPED);
if ((swapped_pins) && (!is_center_aligned))
{
Cy_TCPWM_PWM_SetCompare0(obj->base, obj->resource.channel_num, period - compare);
}
else
{
Cy_TCPWM_PWM_SetCompare0(obj->base, obj->resource.channel_num, compare);
}
return CY_RSLT_SUCCESS;
}
Len
"Engineering is an Art. The Art of Compromise."
- Tags:
- hal
- pwm
- pwm @ 100% dc