Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Len_CONSULTRON
Level 9
Level 9
Beta tester 500 solutions authored 1000 replies posted

I was using HAL PWM code to set the PWM resource to 100% dutycycle.  What I got is that at 100% dutycycle, the PWM turned OFF (effectively 0%).

The issue is actually in the function cyhal_pwm_set_period_and_compare().

This is because:

cyhal_pwm_set_duty_cycle(&obj, 100, frequencyhal_hz)

{

...

     uint32_t period = obj->clock_hz / frequencyhal_hz;

     uint32_t width = (uint32_t)(100 * 0.01f * period);

     cyhal_pwm_set_period_and_compare(obj, period, width);     /* Here period = width @ 100% dc */

     {

     ...

          Cy_TCPWM_PWM_SetPeriod0(obj->base, obj->resource.channel_num, period - 1u);     /* The period count is corrected here */

     ...

     else

     {

          Cy_TCPWM_PWM_SetCompare0(obj->base, obj->resource.channel_num, compare);    

               /* Although the period was corrected (period-1) the compare in this case is period + 1.  The compare count was not corrected. */
               /* When compare > period, the result is an effective 0% dc */

     }

May I recommend the following changes to function cyhal_pwm_set_period_and_compare():

static cy_rslt_t cyhal_pwm_set_period_and_compare(cyhal_pwm_t *obj, uint32_t period, uint32_t compare)

{

    if (period < 1 || period > (uint32_t)((1 << CYHAL_TCPWM_DATA[obj->resource.block_num].max_count)) - 1)

        return CYHAL_PWM_RSLT_BAD_ARGUMENT;

    period = period - 1u;    /* Make the period count correction here. */

                            /* This fixes the issue where period == compare (ie duty_cycle == 100 percent) */

    if (compare > period)

        compare = period;

    cyhal_gpio_t pin = obj->pin;

    cyhal_gpio_t pin_compl = obj->pin_compl;

    Cy_TCPWM_PWM_SetCompare0(obj->base, obj->resource.channel_num, 0u);

    Cy_TCPWM_PWM_SetPeriod0(obj->base, obj->resource.channel_num, period);

    bool swapped_pins = (CY_UTILS_GET_RESOURCE(pin, cyhal_pin_map_tcpwm_line_compl) != NULL) && (CY_UTILS_GET_RESOURCE(pin_compl, cyhal_pin_map_tcpwm_line) != NULL);

    bool is_center_aligned = (TCPWM_CNT_TR_CTRL2(obj->base, obj->resource.channel_num) == CY_TCPWM_PWM_MODE_CNTR_OR_ASYMM) ||

                                (TCPWM_CNT_TR_CTRL2(obj->base, obj->resource.channel_num) == CY_TCPWM_PWM_MODE_CNTR_OR_ASYMM_UO_SWAPPED);

    if ((swapped_pins) && (!is_center_aligned))

    {

        Cy_TCPWM_PWM_SetCompare0(obj->base, obj->resource.channel_num, period - compare);

    }

    else

    {

        Cy_TCPWM_PWM_SetCompare0(obj->base, obj->resource.channel_num, compare);

    }

    return CY_RSLT_SUCCESS;

}

Len

Len
"Engineering is an Art. The Art of Compromise."
0 Likes
2 Replies
DheerajK_81
Moderator
Moderator
Moderator
First comment on KBA First comment on blog 5 questions asked

Hello Len,

Thank you for pointing this out. The fix has been added and you should see it in the next release of the psoc6hal​.

Regards,

Dheeraj

0 Likes
rsiigod
Level 3
Level 3
Distributor - WPG(GC)
25 replies posted 50 sign-ins First solution authored

It seems that the new version still has problems...

I reopen a topic: [Problem] PWM duty setting issue by (PWM-HAL) 

0 Likes