Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
SaGa_4641021
Level 5
Level 5
50 questions asked 50 replies posted 100 sign-ins

Hello

I am trying with small steps to operate the DMA on I2S, so I have an array of 40 values (0 through 0x27) to write to the I2S-TX through DMA. Then I read the I2S-SDO line on logic analyzer.

First, to configure the UDB datapath to be 32-bit wide to have 4-words deep FIFO, do it just configure the data_size to "word" ? or do I have to manually configure some register ?

SaGa_4641021_0-1637986493247.png

I set up the system as follows:

Data to send:    uint32_t txBuff[40]

SaGa_4641021_1-1637986520466.png

DMA: 

SaGa_4641021_2-1637986532857.png

 

I2S:

Tx-only, 24-bits, period 64-bits

SaGa_4641021_3-1637986545915.png

 

DMA:

SaGa_4641021_4-1637986558256.png

 

Result:

In case of I2S set to 16-bits: The output reads 2 consecutive elements from the array at a time, concatenates them and and sends them to the I2S.

SaGa_4641021_5-1637986570162.png

 

In case of I2S set to 24-bits: The output reads 2 consecutive elements from the array at a time, concatenates them and and sends them to the I2S, and skips other some elements in the array:

SaGa_4641021_6-1637986582631.png

 

I expired all the trials and errors and the resources in TRM and datasheets,

Any clue what is wrong with the setup ?

thanks

 

 

0 Likes
1 Solution
RodolfoGL
Employee
Employee
250 solutions authored 250 sign-ins 5 comments on KBA

Because the component was designed for PSoC 4, which has a limited number of UDBs, it uses 8-bit datapath, so you need to write byte by byte to the TX FIFO.  Changing to 32-bit datapath will require some customization, not only on the datapath, but also on the Verilog code and APIs.

I think now I understand why you asked the questions from this case:

https://community.infineon.com/t5/PSoC-6/UDB-I2S-on-PSoC-6/m-p/326004#M11233

To make this work with 8-bit datapath, you need to setup the DMA to transfer byte-to-byte. 

If you need 24-bits, configure the X loop to transfer 3 bytes. And let Y loop to define the number of "words". In your case, that would be 40 words. This how the configuration will look like:

RodolfoGL_0-1638144787453.png

For Y-loop, you need to increment by 4, since your data is stored in a 32-bit array.

Let me know if this works.

 

 

View solution in original post

2 Replies
RodolfoGL
Employee
Employee
250 solutions authored 250 sign-ins 5 comments on KBA

Because the component was designed for PSoC 4, which has a limited number of UDBs, it uses 8-bit datapath, so you need to write byte by byte to the TX FIFO.  Changing to 32-bit datapath will require some customization, not only on the datapath, but also on the Verilog code and APIs.

I think now I understand why you asked the questions from this case:

https://community.infineon.com/t5/PSoC-6/UDB-I2S-on-PSoC-6/m-p/326004#M11233

To make this work with 8-bit datapath, you need to setup the DMA to transfer byte-to-byte. 

If you need 24-bits, configure the X loop to transfer 3 bytes. And let Y loop to define the number of "words". In your case, that would be 40 words. This how the configuration will look like:

RodolfoGL_0-1638144787453.png

For Y-loop, you need to increment by 4, since your data is stored in a 32-bit array.

Let me know if this works.

 

 

lock attach
Attachments are accessible only for community members.
SaGa_4641021
Level 5
Level 5
50 questions asked 50 replies posted 100 sign-ins

i tried your advice and it works, thanks a lot

i attached the code for other to use.