Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

ZaCl_4210281
Level 1
Level 1

I need an example or instruction on how to read a voltage and write it to Gatt DB so I can get it on an app when desired. It's for monitoring a 12v battery level and triggering charge indicators with in the app. How do I do this?

1 Solution

PSoC 6 supports two functions; Cy_BLE_GATTS_WriteAttributeValuePeer and Cy_BLE_GATTS_WriteAttributeValueLocal to trigger attribute write from peer and local device respectively. Please use Cy_BLE_GATTS_WriteAttributeValueLocal for a locally initiated attribute value write.

  • Fill appropriate values in GATT handle value pair.

    /* Local variable that stores handle value pair */

    cy_stc_ble_gatt_handle_value_pair_t  locHandleValuePair =

    {

        .attrHandle = CY_BLE_CS_CUSTOM_CHARACTERISTIC_CHAR_HANDLE,

        .value.len  = 1,

        .value.val  = &bVal

    };

  • Once the ADC conversion is complete, initiate local GATT database write using Cy_BLE_GATTS_WriteAttributeValueLocal. Cy_BLE_GCy_BLE_GATTS_WriteAttributeValueLocalATTS_WriteAttributeValueLocalA

Cy_BLE_GATTS_WriteAttributeValueLocal(&locHandleValuePair);

Please refer to PDL documentation for more details (select PSoC Creator Help > Documentation > Peripheral Driver Library).

View solution in original post

0 Likes
3 Replies
GeonaP_26
Moderator
Moderator
Moderator
250 solutions authored 100 solutions authored 50 solutions authored

You can update the GATT database using CyBle_GattsWriteAttributeValue once the ADC conversion is complete/new data is present. I have appended code snippet for your reference.

    CYBLE_GATT_HANDLE_VALUE_PAIR_T  locHandleValuePair;

    locHandleValuePair.attrHandle = CYBLE_CS_CUSTOM_CHARACTERISTIC_CHAR_HANDLE;

    locHandleValuePair.value.len = 1;

    locHandleValuePair.value.val = &bVal;

    CyBle_GattsWriteAttributeValue( &locHandleValuePair, 0,  &connectionHandle , CYBLE_GATT_DB_LOCALLY_INITIATED );

You can also use the battery service in your application. You can refer to https://www.cypress.com/video-library/PSoC/psoc-4-ble-101-3-add-battery-service/108396

For more details on the CyBle_GattsWriteAttributeValue API, please refer to Updating an Attribute’s Value in GATT DB of a BLE GATT Server - KBA219298

0 Likes

I have basically the same question. I note that the OP applied a tag for "PSOC 063" to their post but the response refers to code and KB articles for PSOC 4.

I also note that the BLE component for the PSoC 6 devices uses different structures and functions with a different naming convention.

Can you please provide example code for a PSoC 6 and/or references to PSoC 6 KB articles?

Susan

0 Likes

PSoC 6 supports two functions; Cy_BLE_GATTS_WriteAttributeValuePeer and Cy_BLE_GATTS_WriteAttributeValueLocal to trigger attribute write from peer and local device respectively. Please use Cy_BLE_GATTS_WriteAttributeValueLocal for a locally initiated attribute value write.

  • Fill appropriate values in GATT handle value pair.

    /* Local variable that stores handle value pair */

    cy_stc_ble_gatt_handle_value_pair_t  locHandleValuePair =

    {

        .attrHandle = CY_BLE_CS_CUSTOM_CHARACTERISTIC_CHAR_HANDLE,

        .value.len  = 1,

        .value.val  = &bVal

    };

  • Once the ADC conversion is complete, initiate local GATT database write using Cy_BLE_GATTS_WriteAttributeValueLocal. Cy_BLE_GCy_BLE_GATTS_WriteAttributeValueLocalATTS_WriteAttributeValueLocalA

Cy_BLE_GATTS_WriteAttributeValueLocal(&locHandleValuePair);

Please refer to PDL documentation for more details (select PSoC Creator Help > Documentation > Peripheral Driver Library).

0 Likes