- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear Community
We are developing 3 Models in 1 product.
for convenience, I want to define a MACRO in the Modus IDE with common code for 3 models.
How to define MACRO in the Modus IDE.
For eg:
If revise the MACRO = MODEL_1,
We can compile the code which is in #if (MODEL == MODEL_1).
If revise the MACRO = MODEL_2,
We can compile the code which is in #if (MODEL == MODEL_2).
If revise the MACRO = MODEL_3,
We can compile the code which is in #if (MODEL == MODEL_3).
Best regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @shiyouxue
Since you have 3 models you can create a MACRO by defining it by:
#define MODEL "MODEL_1"
If the macro is refined as shown, it will execute the code which is in #if (MODEL == "MODEL_1")
For choosing MODEL_2 you can revise the macro by:
#define MODEL "MODEL_2"
Similarly, you can revise it for "MODEL_3"
Thanks and Regards,
Leo