Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

6 Replies
DheerajK_81
Moderator
Moderator
Moderator
First comment on KBA First comment on blog 5 questions asked

Please provide more information on the display you want to use, attach the datasheet if possible. Also, which device and IDE (Creator/ModusToolbox) are you using to create your application?

Regards,

Dheeraj

0 Likes

Thanks for your question, Dheeraj.

I have

- some 1602 ajphanumeric displays (HD44780) with PCF8574T  => I2C Interface

- Waveshare WS13185 with => SPI interface

- ER-TFT M032-3 with ILI9341 => 3 or 4 wire SPI Interface

they all run with PSoC5LP.

Best regards, Wolfgang

0 Likes

I use I2C also but for me it is not clear which devices are NOT working for you.

Mike

0 Likes

Thank you for the input, but you forgot to mention on which device you are trying to migrate to and isn't working.

Regards,

Dheeraj

0 Likes

Hello Dheeraj,

I want to use these displays with the CY8CPROTO-063-BLE kit.

My wish would be to find prefabricated assemblies in the PSoC Creator...

0 Likes