Jul 22, 2021
11:50 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jul 22, 2021
11:50 AM
I want to toggle between 40 pins using the AMUX block which would use the AMUX bus line in PSoC6 and connect the output of the mux to the Tx Pin in the cap sense module. However, I cannot find a simple/intuitive way of doing so - how do I connect the output of the Analog mux to the Capsense block in PSoC Creator? I have already tried to connect the output pin to the Tx pin in cap sense but it doesn't seem like there is a way to do that. Thanks.
Solved! Go to Solution.
Labels
1 Solution
Aug 10, 2021
07:51 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 10, 2021
07:51 PM
Hello @harsh ,
It is not possible to connect the AMUX output to the CapSense block. The logic for multiplexing GPIOs through the AMUX bus is in the code for the CapSense block itself.
Best regards,
Sampath Selvaraj
3 Replies