Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
suno_285741
Level 3
Level 3
10 sign-ins 10 replies posted First solution authored

Hello

I had configured Touch key on PSoC6 (CY8C6245AZI-S3D72)

There is 16 configurable pins for touch. (1 for CMOD, 15 for Touch key)

15 is the maximum number of touch keys?

pastedImage_0.png

0 Likes
1 Solution
Hari
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hello suno_285741

That is correct. PSoC 6 512K part supports CapSense only in port 7, 8 and 9. This imposes a 16 GPIO limitation on these devices. Which means 15 CSD sensors + Cmod.

Note that you can expand the number of sensors by using the CSX sensing method where you can have a matrix arrangement with shared Tx and Rx sensors. CSX takes 2 external caps (CintA and CintB) and the remaining 14 GPIOs can be arranged to 7 Tx + 7 Rx which would give a total of 49 sensing elements.

Thanks,
Hari

View solution in original post

0 Likes
1 Reply
Hari
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hello suno_285741

That is correct. PSoC 6 512K part supports CapSense only in port 7, 8 and 9. This imposes a 16 GPIO limitation on these devices. Which means 15 CSD sensors + Cmod.

Note that you can expand the number of sensors by using the CSX sensing method where you can have a matrix arrangement with shared Tx and Rx sensors. CSX takes 2 external caps (CintA and CintB) and the remaining 14 GPIOs can be arranged to 7 Tx + 7 Rx which would give a total of 49 sensing elements.

Thanks,
Hari

0 Likes