- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I have a project that was created in Modutoolbox 2.1 and I need to use it in modus toolbox 3. I am trying to follow the steps provided in the document KBA236134. In step number 3.1 mentions that is necessary to create a new workspace and in step number 3.2 says to move the existing application to the workspace. after following the document, the document mentions in step 3.3 to add the BSP. When opening the library manager and choosing the app in the application directory says error, the application uses an older build flow. My question here is, Do I have to create a new "empty project in my workspace", add all the source and header files, and then proceed with step number 3.3? As additional information the BSP original project was created for the CY8CPROTO-063-BLE and the new project is also going to be working on the CY8CPROTO-063-BLE evk board.
My second question is if the libraries that I add from the Library manager go to the mtb_shared folder. Because, in my older project all my libraries are located in the lib folder, and the document says in step 3.2 to delete that folder. Should I move them before deleting them to the mtb_shared folder? I have to mention that not all the libraries that I am using are available through the library manager. What should I do there?
If you need more details about my issue, let me know. Thanks in advance!
Regards,
Luis Flores
Solved! Go to Solution.
- Labels:
-
ispn:40049:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Are there other configuration files present in the newly created BSP? If yes, we need to update those files also. According to the app note the linker files should be updated with the settings from the corresponding version 2.x files. All the changes pointed out in the document should be updated as per the appnote.
Thanks and Regards,
Leo
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
For the issue "error, the application uses an older build flow" please refer to section 2: 'Exceptions on backward compatibility' of KBA236134 and the KBA AN235297.
When you add a library from the Library Manager, you can set the type as Local or Shared as described in Library Manager User Guide:
May I ask which libraries you are using that are not available in the library manager?
Thanks and Regards,
Leo
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I will try to check what you shared. About the libraries that I am using, I have in my modus toolbox one that is called bless, another one that is called psoc6hal (I am not sure if mtb-hal-cat1 replaces the one mentioned before), psoc6make (not sure if recipe-make-cat1a replaces it), psoc6pdl (not sure if mtb-pdl-cat1 replaces it). I will try the instructions, and I will come back in case I have some other questions, thanks!
Regards,
Luis
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I am following the AN235297 document, I already created my BSP according to the board I am using (CY8CPROTO-063-BLE). After I finished that, I went to section 4.2 and I am following the steps of 4.2.1 "Using the BSP Assitant tool".
According to the step (BSP configuration files including design.modus, etc.) I just checked the design.modus files and I didn't see any differences. Is there another configuration file other than the design.modus that I have to compare?
I also checked the BSP linker files. In this case, I will upload a Word file with the differences that I found in the "COMPONENT_CM0P" folder files. In the document, there are some screenshots. On the left side are located the files that correspond to the Modus Toolbox project, and on the right side are the ones located in the new BSP created for Modus Toolbox 3.0. I highlighted in red the differences I found. How do I know what changes I have to do in the BSP created for ModusToolbox 3.0?
To finish this comment. For the linker files do I only have to compare the files included in the "COMPONENT_CM0P" and the files included in the "COMPONENT_CM4"?
I attached the Word file to this reply. I´ll be waiting for your help, thanks and I appreciate your support!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Are there other configuration files present in the newly created BSP? If yes, we need to update those files also. According to the app note the linker files should be updated with the settings from the corresponding version 2.x files. All the changes pointed out in the document should be updated as per the appnote.
Thanks and Regards,
Leo
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @ESCLuisFlores ,
Thread was locked due to inactivity for long time, you can continue the discussion on the topic by opening a new thread with reference to the locked one. The continuous discussion in an inactive thread may mostly be unattended by community users.
Thanks and Regards,
Leo