Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
KeSh_1984591
Level 2
Level 2
10 replies posted 5 replies posted 5 questions asked

Hi Everyone,

I am currently programming on PSOC CY8C6137BZI-F54 . My majority work is for the analog DAC and current source. I tried making the schematic attached with this post. While building the code I receive the error mentioned below.

"Net "Net_261" is connected to analog mux "AMux_3" and analog mux "AMux_2", but it may connect to only one analog mux when it is an analog mux common connection."

Also I wanted to ask the analog multiplexer can also work as de-multiplexer? Please help me on this.

0 Likes
1 Solution
Vasanth
Moderator
Moderator
Moderator
250 sign-ins 500 solutions authored First question asked

Hi,

There is  a restriction in sequencing the Amux components. So you cannot connect them in series. You can try to clone or buffer the common signal to avoid this problem as specified. To answer your second question, Amux can act as a de-multiplexer too.

Best Regards,
Vasanth

View solution in original post

2 Replies
lock attach
Attachments are accessible only for community members.
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
First comment on blog Beta tester First comment on KBA

Hi,

Since I am not an Analog expert, I may be missing your point.

But only to connect analog routing, we could draw schematic like

001-schematic-1.JPG

But in my understanding, ADC can't measure current directly,

we may need to connect resistors of "known" value to each pins

so that we can calculate the current from the voltage.

002-schematic-2.JPG

And adding another idea sketch, ADC also could have multiple input.

003-schematic-3.JPG

moto

0 Likes
Vasanth
Moderator
Moderator
Moderator
250 sign-ins 500 solutions authored First question asked

Hi,

There is  a restriction in sequencing the Amux components. So you cannot connect them in series. You can try to clone or buffer the common signal to avoid this problem as specified. To answer your second question, Amux can act as a de-multiplexer too.

Best Regards,
Vasanth