- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I try to implement 2 alarms with the RTC component on the PSOC6,
My issue it's when I call 2 functions to Set the 2 different alarms :
rtcApiResult = Cy_RTC_SetAlarmDateAndTime(&alarm1,CY_RTC_ALARM_1);
rtcApiResult = Cy_RTC_SetAlarmDateAndTime(&alarm2,CY_RTC_ALARM_2);
I got the good return for the first function, but an error for the second (CY_RTC_INVALID_STATE)
If I put a CyDelay(1) between the 2 functions, I don't have any trouble
My question is : how to set the 2 alarms correctly (use the delay it's maybe not the good way to do it)
Thank you
Solved! Go to Solution.
- Labels:
-
PSoC 6 MCU
- Tags:
- Alarms
- psoc 6 mcu
- rtc
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
It is recommended to put a delay else RTC will be busy.
This is shown in the below code snippet.
/* RTC Write bit set is possible only in condition that CY_RTC_BUSY bit = 0
* or RTC Read bit is not set
*/
if ((CY_RTC_BUSY != Cy_RTC_GetSyncStatus()) && (!_FLD2BOOL(BACKUP_RTC_RW_READ, BACKUP_RTC_RW)))
{
BACKUP_RTC_RW |= BACKUP_RTC_RW_WRITE_Msk;
retVal = CY_RTC_SUCCESS;
}
}
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
It is recommended to put a delay else RTC will be busy.
This is shown in the below code snippet.
/* RTC Write bit set is possible only in condition that CY_RTC_BUSY bit = 0
* or RTC Read bit is not set
*/
if ((CY_RTC_BUSY != Cy_RTC_GetSyncStatus()) && (!_FLD2BOOL(BACKUP_RTC_RW_READ, BACKUP_RTC_RW)))
{
BACKUP_RTC_RW |= BACKUP_RTC_RW_WRITE_Msk;
retVal = CY_RTC_SUCCESS;
}
}
Regards