Dual core application with custom BSP - hex file issue

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
prk_4086136
Level 3
Level 3
25 sign-ins 25 replies posted 10 replies posted

Hello,

I made a custom BSP for my part CY8C6347FMI-BLD33, and started a new dual core application using the example. I am able to successfully compile and build output.
But there is a discrepancy between my build summary and actual hex files. PFA.

The build summary output is correct, but in the hex files, the flash addresses are overlapping. 

Not able to figure out why this is happening, please help.

(Note: When I implemented UART code in both cores, it worked well. But when I integrate Bluetooth stack in CM0p, the compilation was not working citing that the cm0p and cm4p hex output are overlapping)

0 Likes
1 Reply
Ekta
Moderator
Moderator
Moderator
750 replies posted First like given 250 solutions authored

Hi @prk_4086136 

I see that the hex files for both cm0p and cm4 start from the same address. Looks like this might be due to linker script configuration for your project.


Can you zip the entire project and attach it on this thread so that we can verify that all the settings are correctly made?

Best Regards
Ekta

0 Likes