- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Team,
We are designing a board using the MCU CY8C6247FTI-D52T.
1 x UART = SCB7, TX - P1[0], RX - P1[1]
2 x I2C = SCB5, SCL - P5[0], SDA - P5[1]
SCB8, SCL - P6[0], SDA - P6[1]
16 x GPIO
3 x Analog Read = P10[1], P10[4], P10[5]
1 x Analog Write = P10[0]
are used.
SWD is the debugging interface. -
SWDIO - P6[6]
SWCLK - P6[7]
XRES
SWO - P6[4]
32KHz RTC OScillator - P0[0], P0[1]
High-speed oscillator - P12[6], P12[7]
The schematic is attached herewith.
Please let me know if there are any mistakes.
Solved! Go to Solution.
- Labels:
-
PSoC 6 MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @shibin,
I have gone through your schematic and the following are my observations:
- Pin connections are correct.
- SCB blocks are used correctly.
- Only connect 4.7 uF capacitor close to the VBUCK1 and for the VCCD just short it with VBUCK1 (C53, 56 and 57 are not required)
- VDDA has an additional 1 uF capacitor, which is not required.
- The VBACKUP doesn’t require a 10uF capacitor.
- It is recommended to use a 330-Ohm series resistance directly connected to the pin before 4.7 kOhm Pull up resistance for i2c.
- For DEBUG interface if you are using 10 pin connector then connect all signals required for it as given in “PSoC 6 Hardware Design Consideration”
- For i) ECO P12.6 = ECO_IN, P12.7 = ECO_OUT ii) WCO P0.0 = WCO_IN, P0.1 = WCO_OUT
Please, let me know if any further clarification is required.
Thank you
Best Regards
Raj Chaudhari
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @shibin,
I have gone through your schematic and the following are my observations:
- Pin connections are correct.
- SCB blocks are used correctly.
- Only connect 4.7 uF capacitor close to the VBUCK1 and for the VCCD just short it with VBUCK1 (C53, 56 and 57 are not required)
- VDDA has an additional 1 uF capacitor, which is not required.
- The VBACKUP doesn’t require a 10uF capacitor.
- It is recommended to use a 330-Ohm series resistance directly connected to the pin before 4.7 kOhm Pull up resistance for i2c.
- For DEBUG interface if you are using 10 pin connector then connect all signals required for it as given in “PSoC 6 Hardware Design Consideration”
- For i) ECO P12.6 = ECO_IN, P12.7 = ECO_OUT ii) WCO P0.0 = WCO_IN, P0.1 = WCO_OUT
Please, let me know if any further clarification is required.
Thank you
Best Regards
Raj Chaudhari