Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 6 Forum Discussions

shibin
Level 1
Level 1
5 replies posted 5 sign-ins First like received

Hi Team,
       We are designing a board using the MCU CY8C6137BZI-F14
      1 x UART = SCB7, TX - P1[1], RX - P1[0]
      2 x I2C = SCB5, SCL - P5[0], SDA - P5[1]
                          SCB8, SCL - P6[0], SDA - P6[1]
      16 x GPIO
       3 x Analog Read = P10[1], P10[4], P10[5] 
       1 x Analog Write = P10[0]
       SWD is the debugging interface. -
       SWDIO - P6[6]
      SWCLK - P6[7]
      XRES
      SWO - P6[4]
      32KHz RTC OScillator - P0[0], P0[1]
      High-speed oscillator - P12[6], P12[7]
1). I hope the pin mapping is correct
2). I believe the ECO and the WCO pins are correct and their load capacitors.
        The crystal for WCO used is - CM9V-T1A-32.768KHZ-12.5PF-20PPM-TA-QC its load capacitance is 12.5pF.
        The crystal used for  ECO is - LFXTAL063075BULK, load capacitance - 22pF
3). The VBACKUP pin is supplied from the same source that powers the VDDD pin.
4). We are not using a USB, so the pin VDDUSB has connected to the same power supply that powers the VDDD pin.
5). Only a 1uF decoupling capacitor is used at the VREF pin
6). Only a 10uF decoupling capacitor is placed at the VRF pin.
7). Could you please suggest to e a programmer and the development kit for the select MCU.
     I hope this will suffice. 
 DEV KIT - PSoC® 6 WiFi-BT Pioneer Kit (CY8CKIT-062-WiFi-BT) (cypress.com)
                                                     Programmer -  CY8CKIT-005 MiniProg4 Program and Debug Kit (cypress.com)

The schematic is attached herewith.
Please let me know if there are any mistakes.

0 Likes
1 Solution
Raj_JC
Moderator
Moderator
Moderator
250 replies posted First question asked 100 solutions authored

Hi @shibin,

I have given the solution to this in the newer thread "https://community.infineon.com/t5/PSoC-6/Desiging-with-CY8C6137BZI-F14/td-p/323630"

I am going to lock this thread as it is a duplicate. Please feel free to continue the discussion in a newer thread.

Thank you

Best Regards 

Raj Chaudhari

 

View solution in original post

0 Likes
2 Replies
shibin
Level 1
Level 1
5 replies posted 5 sign-ins First like received

Hi Team,
Any updates on the same

0 Likes
Raj_JC
Moderator
Moderator
Moderator
250 replies posted First question asked 100 solutions authored

Hi @shibin,

I have given the solution to this in the newer thread "https://community.infineon.com/t5/PSoC-6/Desiging-with-CY8C6137BZI-F14/td-p/323630"

I am going to lock this thread as it is a duplicate. Please feel free to continue the discussion in a newer thread.

Thank you

Best Regards 

Raj Chaudhari

 

0 Likes