Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 6

AyKo_4382201
Level 2
10 replies posted 5 replies posted 5 questions asked
Level 2

Hey,

I'm using CYBLE-416045-02 ble. For testing purpose I'm sending a 2 byte response into to a only read Response characteristic.

I'm able to get data from the ble app but cant send the 2 byte response.Please help.

Thankyou

0 Likes
1 Solution
Yugandhar
Moderator
Moderator First comment on blog 750 replies posted 500 replies posted
Moderator

Hello,

Could you please refer to the below attached sample project. In this project, if you write two bytes of data from the central device then the values will be updated into the GATT DB at peripheral device. And, the updated values will be displayed in Central device through read response.

Please let me know if this helps.

Thanks,

P Yugandhar.

View solution in original post

0 Likes
6 Replies
Yugandhar
Moderator
Moderator First comment on blog 750 replies posted 500 replies posted
Moderator

Hello,

Could you please refer to the below attached sample project. In this project, if you write two bytes of data from the central device then the values will be updated into the GATT DB at peripheral device. And, the updated values will be displayed in Central device through read response.

Please let me know if this helps.

Thanks,

P Yugandhar.

0 Likes
AyKo_4382201
Level 2
10 replies posted 5 replies posted 5 questions asked
Level 2

Hi,

Thanks for replying. The project you have shared with me has errors as you can see in below attached image.Screenshot (6).png

0 Likes
Yugandhar
Moderator
Moderator First comment on blog 750 replies posted 500 replies posted
Moderator

Hello,

I'm able to open the project at my end. Could you please try downloading again ?

Thanks,

P Yugandhar.

0 Likes
AyKo_4382201
Level 2
10 replies posted 5 replies posted 5 questions asked
Level 2

Hi,

Thanks, your project work fine. But i still have some questions:-

1) I have 2 characteristics named command (write only) and response (read only).

2) I'm able to communicate between psoc6 and mobile app only when i make response characteristic(which should be read only)  both read and write.

0 Likes
AyKo_4382201
Level 2
10 replies posted 5 replies posted 5 questions asked
Level 2

Continued...

Why am I not able to communicate both ways (app and psoc6) when i configure response characteristics as read only?

0 Likes
AyKo_4382201
Level 2
10 replies posted 5 replies posted 5 questions asked
Level 2

Thanks my problem has been solved.It was a typo error, I was using CY_BLE_SMARTDOOR_READ_PACKET_CHAR_INDEX instead of CY_BLE_SMARTDOOR_READ_PACKET_CHAR_HANDLE.

Again thanks for the help.