I'd like to try PI DYN in a datapath, but it's grayed out in the datapath configuration tool:
I understand that to actually use PI dynamically, I also have to set CFB EN for the given instruction in CFGRAM, because CFB EN and PI DYN are ANDed, and I'd have to switch PI SEL back to ACC:
But how do I set PI DYN?
Solved! Go to Solution.
The PI DYN bit is disabled by default. You can enable it by right-clicking on the bit and select "Enable bit" as shown in below screenshot:
Also, this app note - AN82156 Designing PSoC Creator Components with UDB Datapaths ( https://www.cypress.com/file/41531/download ) contains an example of using datapath Parallel In - Parallel Out, which may help ( Project #5 – Parallel In and Parallel Out )
Best Regards,
Prem Sai
The PI DYN bit is disabled by default. You can enable it by right-clicking on the bit and select "Enable bit" as shown in below screenshot:
Also, this app note - AN82156 Designing PSoC Creator Components with UDB Datapaths ( https://www.cypress.com/file/41531/download ) contains an example of using datapath Parallel In - Parallel Out, which may help ( Project #5 – Parallel In and Parallel Out )
Best Regards,
Prem Sai