Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
HeLi_1220176
Level 1
Level 1
5 sign-ins First comment on KBA 5 questions asked

On the

CY8CPROTO-063-BLE there is an external crystal 32mhz (ECO) and a watch crystal WCO.  Are these actually necessary or just optional for making use of the module?  Seems there's already internal crystal oscillator.

Also can USB interface be used on

CY8CPROTO-063-BLE by routing some pins?  I think not but just double checking.

0 Likes
1 Solution

HeLi_1220176

The BLE ECO is mandatory for BLE functionality, and BLE ECO is already mounted inside CYBLE-416045-02. The ECO is different from the BLE ECO. They have different IO pins.

However, the main system clock can be sourced from BLE ECO if it's already there, therefore, the ECO could be omitted in this case.

As for the WCO, you need connect it outside the module.

That's the reason you may see Y1 is not loaded and Y2 is there on CY8CPROTO-063-BLE board.

View solution in original post

2 Replies
Len_CONSULTRON
Level 9
Level 9
Beta tester 500 solutions authored 1000 replies posted

HeLi,

The ECO is needed to provide an accurate BLE frequencies +/- 100ppm or less.  BLE frequencies need this accuracy or the other end of the BLE connection will not connect reliably.    The WCO is potentially not necessary depending on the BLE  message mode you are using.  It is necessary for many of the BLE message modes which require +/-100ppm accuracy.

Len

Len
"Engineering is an Art. The Art of Compromise."
0 Likes

HeLi_1220176

The BLE ECO is mandatory for BLE functionality, and BLE ECO is already mounted inside CYBLE-416045-02. The ECO is different from the BLE ECO. They have different IO pins.

However, the main system clock can be sourced from BLE ECO if it's already there, therefore, the ECO could be omitted in this case.

As for the WCO, you need connect it outside the module.

That's the reason you may see Y1 is not loaded and Y2 is there on CY8CPROTO-063-BLE board.