Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
YeJE_3763896
Level 1
Level 1
First like given Welcome!

HELLO, I am making a BLE MODULE using CY8C6336BZI-BLF03.

I asked yesterday, I have another question today

(plz check the attached file first.)

I don't use the "VTARG". So, Do not need to the attached schematic? Do I have need to use that?

If using that, can I change "VDD_NS" to "VDDR" ?

Thank you for your time and prompt response

0 Likes
1 Solution
VenkataD_41
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi,

There is no need to connect the VTARG as shown in the image attached.

Please note that VDD_NS should be connected to VDDD and also a 10 uF decoupling capacitor should be connected on VDD_NS.

If you are using BLE please check the connections for VDDR1, VDDR2 and VDDR3 in page number 20 of the PSoC 63 device datasheet.

http://www.cypress.com/file/385921/download

Thanks

Ganesh

View solution in original post

0 Likes
1 Reply
VenkataD_41
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi,

There is no need to connect the VTARG as shown in the image attached.

Please note that VDD_NS should be connected to VDDD and also a 10 uF decoupling capacitor should be connected on VDD_NS.

If you are using BLE please check the connections for VDDR1, VDDR2 and VDDR3 in page number 20 of the PSoC 63 device datasheet.

http://www.cypress.com/file/385921/download

Thanks

Ganesh

0 Likes