公告

大中华汽车电子生态圈社区并入开发者社区- 更多资讯点击此

Tip / 登入 to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Frank_vec
Level 4
Level 4
Distributor - Zenitron(GC)
50 replies posted First like received First comment on blog

1、使用modus 建立Bluetooth_LE_Battery_Server 项目

2、CY_USING_PREBUILT_CM0P_IMAGE 这个宏定义具体含义是啥呀 ?

 

不胜感激

0 点赞
1 解答
Vison_Zhang
Moderator
Moderator
Moderator
First comment on KBA 750 replies posted 250 sign-ins

这个 mtb_shared/psoc6cm0p/release-vx.x.x/README.md 中解释。我把部分内容拷贝了出来,你可以读一下。

# PSoC 6 Cortex M0+ prebuilt images

### Overview

Prebuilt application images are executed on the Cortex M0+ core of the PSoC 6 dual-core MCU.
The images are provided as C arrays ready to be compiled as part of the Cortex M4 application.
The Cortex M0+ application code is placed to internal flash by the Cortex M4 linker script.

Note: Each application image has a variant based on the hardware die (e.g.
psoc6_01, psoc6_02, psoc6_03, ...) it is supported on. An #ifdef at the top of
each .c file automatically controls which version is used so there is no need
to specify a particular image.

### Images

* [COMPONENT_CM0P_SLEEP](./COMPONENT_CM0P_SLEEP/README.md)

    This image starts CM4 core at CY_CORTEX_M4_APPL_ADDR=0x10002000
    and puts CM0+ core into a deep sleep mode.

* [COMPONENT_CM0P_CRYPTO](./COMPONENT_CM0P_CRYPTO/README.md)

    This image starts crypto server on CM0+ core,
    starts CM4 core at CY_CORTEX_M4_APPL_ADDR=0x10008000
    and puts CM0+ core into a deep sleep mode.

* [COMPONENT_CM0P_BLESS](./COMPONENT_CM0P_BLESS/README.md)

    This image starts BLE controller on CM0+ core,
    starts CM4 core at CY_CORTEX_M4_APPL_ADDR=0x10020000
    and puts CM0+ core into a deep sleep mode.

* [COMPONENT_CM0P_SECURE](./COMPONENT_CM0P_SECURE/README.md)

    This image starts CM4 core at address corresponding
    to Secure Boot policy, sets required security settings,
    initializes and executes code of Protected Register Access
    driver, puts CM0+ core into a deep sleep mode.

在原帖中查看解决方案

0 点赞
6 回复数
Vison_Zhang
Moderator
Moderator
Moderator
First comment on KBA 750 replies posted 250 sign-ins

这个 mtb_shared/psoc6cm0p/release-vx.x.x/README.md 中解释。我把部分内容拷贝了出来,你可以读一下。

# PSoC 6 Cortex M0+ prebuilt images

### Overview

Prebuilt application images are executed on the Cortex M0+ core of the PSoC 6 dual-core MCU.
The images are provided as C arrays ready to be compiled as part of the Cortex M4 application.
The Cortex M0+ application code is placed to internal flash by the Cortex M4 linker script.

Note: Each application image has a variant based on the hardware die (e.g.
psoc6_01, psoc6_02, psoc6_03, ...) it is supported on. An #ifdef at the top of
each .c file automatically controls which version is used so there is no need
to specify a particular image.

### Images

* [COMPONENT_CM0P_SLEEP](./COMPONENT_CM0P_SLEEP/README.md)

    This image starts CM4 core at CY_CORTEX_M4_APPL_ADDR=0x10002000
    and puts CM0+ core into a deep sleep mode.

* [COMPONENT_CM0P_CRYPTO](./COMPONENT_CM0P_CRYPTO/README.md)

    This image starts crypto server on CM0+ core,
    starts CM4 core at CY_CORTEX_M4_APPL_ADDR=0x10008000
    and puts CM0+ core into a deep sleep mode.

* [COMPONENT_CM0P_BLESS](./COMPONENT_CM0P_BLESS/README.md)

    This image starts BLE controller on CM0+ core,
    starts CM4 core at CY_CORTEX_M4_APPL_ADDR=0x10020000
    and puts CM0+ core into a deep sleep mode.

* [COMPONENT_CM0P_SECURE](./COMPONENT_CM0P_SECURE/README.md)

    This image starts CM4 core at address corresponding
    to Secure Boot policy, sets required security settings,
    initializes and executes code of Protected Register Access
    driver, puts CM0+ core into a deep sleep mode.
0 点赞
Frank_vec
Level 4
Level 4
Distributor - Zenitron(GC)
50 replies posted First like received First comment on blog

Frank_vec_0-1679039337542.png

 

 

你好,按照您说的 ,没有找到更多信息 

CY_USING_PREBUILT_CM0P_IMAG   也没有这个的更多信息

 

谢谢 

 

0 点赞
Vison_Zhang
Moderator
Moderator
Moderator
First comment on KBA 750 replies posted 250 sign-ins

“Prebuilt application images are executed on the Cortex M0+ core of the PSoC 6 dual-core MCU. The images are provided as C arrays ready to be compiled as part of the Cortex M4 application. The Cortex M0+ application code is placed to internal flash by the Cortex M4 linker script”  这不就是解释吗。 你想要什么样的解释。

0 点赞
Frank_vec
Level 4
Level 4
Distributor - Zenitron(GC)
50 replies posted First like received First comment on blog

👍👍

0 点赞
Vison_Zhang
Moderator
Moderator
Moderator
First comment on KBA 750 replies posted 250 sign-ins

举个简单的例子,MTB中一个 BLE 的例子工程,默认不会创建成一个 dual-project 的工程(cm0p 和 cm4 各有一个独立的工程,各有一个main.c),而是一个 combined 的工程,只有一个 main.c,那如何让 BLESS 工作在 dul-cpu mode, 让 CM0P 和 CM4 和分别分担 BLE 的部分工作呢。现在给出的方法就是将 CM0P 执行的那部分 BLE 的功能的代码以 pre-image 的方式保存下来,然后在编译 CM4 核的 image 的时候,通过修改 makefile 将 cm0p bless 的那部分 image 与 cm4 的 image 连接起来,最后组成一个 HEX 文件。虽然是一个 HEX 文件,但其实包含了 cm0p image 和 cm4 image 两部分内容,这样两个核就可以一起工作,让 BLE 工作的 dual-cpu 模式.

 

一下是官方文件对  BLESS Pre-image 的原理和用法的解释

 

Pre-compiled BLESS Controller image executed on the Cortex M0+ core of the PSoC 6 dual-core MCU.
The image is provided as C array ready to be compiled as part of the Cortex M4 application.
The Cortex M0+ application code is placed to internal flash by the Cortex M4 linker script.

This image is used only in BLE dual CPU mode. In this mode, the BLE functionality is split between
CM0+ (controller) and CM4 (host). It uses IPC for communication between two CPU cores where both the
controller and host run:

    -------------------------------          ------------------------------------
    |    CM0p (pre-built image)   |          |              CM4                 |
    | --------------------  ----- |          | -----  ------------------------  |
    | |                  |  | H | |   IPC    | |   |  |  BLE Application     |  |
    | | BLE Controller   |--| c | |<-------->| |   |  ------------------------  |
    | |       (LL)       |  | I | |(commands,| |   |          |            |    |
    | |                  |  ----- |  events) | |   |  -----------------    |    |
    | --------------------        |          | | H |  |  BLE Profiles |    |    |
    -------------------------------          | | C |  -----------------    |    |
                  |                          | | I |          |            |    |
       ------------------------              | |   |  ------------------------- |
       |       BLE HW         |              | |   |--|  BLE Host (GAP, L2CAP,| |
       ------------------------              | |   |  |  SM, ATT)             | |
                                             | |   |  ------------------------- |
                                             | -----                            |
                                             ------------------------------------


BLESS Controller pre-built image executes the following steps:
- configures BLESS interrupt
- registers IPC-pipe callback for BLE middleware; the BLE middleware uses this callback to
  initialize and enable the BLE controller when BLE middleware operates in BLE dual CPU mode
- starts CM4 core at CY_CORTEX_M4_APPL_ADDR=0x10020000
- goes to the while loop where processes BLE controller events and puts the CM0+ core into Deep Sleep.

### Usage
To use this image, update the ram, flash, and FLASH_CM0P_SIZE values in the linker script for CM4:
```
Example for the GCC compiler:
...
MEMORY
{
	...
	ram       (rwx)   : ORIGIN = 0x08003000, LENGTH = 0x044800
	flash     (rx)    : ORIGIN = 0x10000000, LENGTH = 0x100000
	...  
}
...
/* The size and start addresses of the Cortex-M0+ application image */
FLASH_CM0P_SIZE  = 0x20000;
...
```
```
Example for the IAR compiler:
...
/* RAM */
define symbol __ICFEDIT_region_IRAM1_start__ = 0x08003000;
define symbol __ICFEDIT_region_IRAM1_end__   = 0x08047800;
/* Flash */
define symbol __ICFEDIT_region_IROM1_start__ = 0x10000000;
define symbol __ICFEDIT_region_IROM1_end__   = 0x10100000;
...
/* The size and start addresses of the Cortex-M0+ application image */
define symbol FLASH_CM0P_SIZE  = 0x20000;
...
```
```
Example for ARMC6 compiler:
...
; RAM
#define RAM_START               0x08003000
#define RAM_SIZE                0x00044800
; Flash
#define FLASH_START             0x10000000
#define FLASH_SIZE              0x00100000
...
/* The size and start addresses of the Cortex-M0+ application image */
#define FLASH_CM0P_SIZE         0x20000
...
```

To use this image in the custom BSP, adjust the BSP target makefile to
add the COMPONENT_CM0P_BLESS directory to the list of components
discovered by ModusToolbox build system:

```
COMPONENTS+=CM0P_BLESS
```

Also, to operate in Dual CPU mode, add the COMPONENT_BLESS_HOST_IPC directory to 
the list of the application level Makefile components:

```
COMPONENTS+=BLESS_HOST_IPC
```
Make sure there is a single CM0P_* component included in the COMPONENTS list

 

0 点赞
Frank_vec
Level 4
Level 4
Distributor - Zenitron(GC)
50 replies posted First like received First comment on blog

非常感谢您的帮助,我受益良多,以后我慢点仔细看答案,谢谢

0 点赞