I am referring "CE220960" project to implement "Upgradable Stack Bootloader" and it works fine when used as it is, with complete BLE running on single core CM4. My requirement is to use BLE on dual core (controller on CM0+ and Host and Profiles on CM4). But after making modifications as per "Appendix A: BLE Component CPU Core Configuration" of CE220960.pdf file, when I click Clean and Build all projects as mentioned in pdf errors are generated in 'Stack application' and 'user application' project. I have attached workspace below with all necessary modifications for dual core "Upgradable Stack Bootloader" which also generate errors after building the projects.
Solved! Go to Solution.
Dual-CPU configuration will be supported in Upgradable Stack Bootloader CE from the next revision (*A). Apologies for the inconvinience.
Dual-CPU configuration will be supported in Upgradable Stack Bootloader CE from the next revision (*A). Apologies for the inconvinience.