- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Using https://infineon.github.io/dfu/dfu_sdk_api_reference_manual/html/index.html#ssection_dfu_step_4
App1 will not compile:
- address 0x10061090 of ...elf section `.text' is not within region `flash_app1'
- section `.ARM.exidx' will not fit in region `flash_app1'
The dfu_cm4_app1.ld file provided has:
flash_app0 (rx) : ORIGIN = 0x10002000, LENGTH = 0x10000
flash_app1 (rx) : ORIGIN = 0x10050000, LENGTH = 0x10000
flash_boot_meta (rw) : ORIGIN = 0x100FFA00, LENGTH = 0x400
I think this is wrong, for 2 reasons:
- There is wasted flash between 0x10012000 and 0x10050000
- The 1MB flash is not fully used. App1 should extend to flash_boot_meta 0x100FFA00
Therefore, I believe the correct line is
flash_app1 (rx) : ORIGIN = 0x10012000, LENGTH = 0xEDA00
Questions:
- Is there any reason to leave the 0x10012000 and 0x10050000 unused?
- Is the new size valid?
- Does the change only have to be made in the dfu_cm4_app0.ld, and dfu_cm4_app1.ld files, or which others?
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
1. LENGTH and START are configurable. It is not mandatory to leave spaces b/w APPs
2. Yes EDA00 is valid - App2 is using complete available flash now (Total Flash = App1 Suez = Meta data + App2 size)
3. Only linker files (.ld) need to be updated.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
1. LENGTH and START are configurable. It is not mandatory to leave spaces b/w APPs
2. Yes EDA00 is valid - App2 is using complete available flash now (Total Flash = App1 Suez = Meta data + App2 size)
3. Only linker files (.ld) need to be updated.