- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Team Cypress,
I am here to ask for your recommendation on
the best Cypress MCU or/and Evaluation Board that can control 3.98 inch LCD touchscreen and more features,
in order to develop touch screen device.
The client was considering the following ST-micro MCU before,
because of its simple guidance to the sample project guide.
https://www.st.com/en/microcontrollers-microprocessors/stm32g0b1ke.html
MCU Specifications in need :
-supports LCD : 3.98 inch, 320X480, RGB, 40pin
(ILI9488, a-Si TFT LCD single chip driver : https://focuslcds.com/content/ILI9488.pdf )
-supports 2D graphics acceleration
-supports single touch feature (capacitive)
-supports PWM controllers for buzzer feature for audio
-better than Arm Cortex-M0+
-32-bit MCU
-6x USART, timers
-ADC, DAC
-comm. I/Fs
-1.7-3.6V
-RAM size : 144kB or better
-Flash size : 256kB or 512kB
-compatible to use NAND flash of size 4~8MB
(in order for the device to support user interface in
three different languages(Korean, Chinese, English))
-preferably has easy development environment to develop the LCD touchscreen device.
If you can recommend MCU or/and evaluation board that can support above feature with design guidance for LCD touch device project, that would be greatly appreciated to share it with the client.
As always, thank you for your considerations to help and bring our business forward.
Ben
Solved! Go to Solution.
- Labels:
-
PSoC 6 MCU
- Tags:
- capsense
- evaluation board
- LCD control
- mcu
- PSoC 4 MCU
- PSoC 5 MCU
- PSoC™ Automotive Multitouch
- touchscreen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @benkim
Please take a look at our PSoC 6 devices. They support the CapSense IP for capacitive touch sensing. We have devices with 256k, 512k, 1MB and 2MB of flash.
They are dual-core processors with CM0+ and CM4 processors.
These also support the EMWIN library for TFT displays.
You can take a look at the PSoC 62 datasheet for more information - https://www.cypress.com/file/385916/download
You can also take a look at the PSoC 62 WiFi-BT kit which comes with the PSoC 62 device and has a 2.4inch 240x320 display already included. https://www.cypress.com/documentation/development-kitsboards/psoc-6-wifi-bt-pioneer-kit-cy8ckit-062-...
Best regards,
Hari