There are two linker script files, cy8c6xx7_cm4_dual.ld and cy8c6xx7_cm0plus.ld
You can change the configuration at the MEMORY section in both linker script files like as following.
MEMORY
{
/* The ram and flash regions control RAM and flash memory allocation for the CM4 core.
* You can change the memory allocation by editing the 'ram' and 'flash' regions.
* Note that 2 KB of RAM (at the end of the RAM section) are reserved for system use.
* Using this memory region for other purposes will lead to unexpected behavior.
* Your changes must be aligned with the corresponding memory regions for CM0+ core in 'xx_cm0plus.ld',
* where 'xx' is the device group; for example, 'cy8c6xx7_cm0plus.ld'.
*/
ram (rwx) : ORIGIN = 0x08024000, LENGTH = 0x23800
flash (rx) : ORIGIN = 0x10080000, LENGTH = 0x80000
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I have built the code example UART_Low_Level_DMA and checked the MAP files.
There are two MAP files, one for CM4 and another one for M0+.
The map file for CM4 has following configuration.
Memory Configuration
Name Origin Length Attributes
ram 0x08024000 0x00023800 xrw
flash 0x10080000 0x00080000 xr
em_eeprom 0x14000000 0x00008000 xr
sflash_user_data 0x16000800 0x00000800 xr
sflash_nar 0x16001a00 0x00000200 xr
sflash_public_key 0x16005a00 0x00000c00 xr
sflash_toc_2 0x16007c00 0x00000200 xr
sflash_rtoc_2 0x16007e00 0x00000200 xr
xip 0x18000000 0x08000000 xr
efuse 0x90700000 0x00100000 r
*default* 0x00000000 0xffffffff
The CM4 uses SRAM from 0x08024000 to 0x080477FF
The map file for CM0+ has following configuration.
Memory Configuration
Name Origin Length Attributes
ram 0x08000000 0x00024000 xrw
flash 0x10000000 0x00080000 xr
em_eeprom 0x14000000 0x00008000 xr
sflash_user_data 0x16000800 0x00000800 xr
sflash_nar 0x16001a00 0x00000200 xr
sflash_public_key 0x16005a00 0x00000c00 xr
sflash_toc_2 0x16007c00 0x00000200 xr
sflash_rtoc_2 0x16007e00 0x00000200 xr
xip 0x18000000 0x08000000 xr
efuse 0x90700000 0x00100000 r
*default* 0x00000000 0xffffffff
The CM0+ uses SRAM from 0x08000000 to 0x08023FFF
Because the RxDmaUartBufferA[] array is declared in the main_cm4.c source code for CM4, the array is located at the SRAM from 0x08024000 to 0x080477FF
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
thanks, if i want to change the CM4 start SRAM address, What should we do? Can you give me the documents about SRAM distribution CM0 and CM4 。
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
There are two linker script files, cy8c6xx7_cm4_dual.ld and cy8c6xx7_cm0plus.ld
You can change the configuration at the MEMORY section in both linker script files like as following.
MEMORY
{
/* The ram and flash regions control RAM and flash memory allocation for the CM4 core.
* You can change the memory allocation by editing the 'ram' and 'flash' regions.
* Note that 2 KB of RAM (at the end of the RAM section) are reserved for system use.
* Using this memory region for other purposes will lead to unexpected behavior.
* Your changes must be aligned with the corresponding memory regions for CM0+ core in 'xx_cm0plus.ld',
* where 'xx' is the device group; for example, 'cy8c6xx7_cm0plus.ld'.
*/
ram (rwx) : ORIGIN = 0x08024000, LENGTH = 0x23800
flash (rx) : ORIGIN = 0x10080000, LENGTH = 0x80000