- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,I purchased an EVB - cy8ckit-062s2-43012
At first I programed a sample project and it worked fine.
Then when I try to program another project it writes me an error (the debug notes bellow) and I can not burn at all
Even when I tried with the PSOC CREATOR/PROGRAMER it did not recognize the PSOC6 CPU
The project that burned into the micro works so that the micro did not stop working.
any idea what is the problem ?
thanks !
- Labels:
-
ispn:39621:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @rahul_2464,
Can you please let me know the application that you programmed into the device? I do not see the logs attached. Can you please reattach the logs?
Even when I tried with the PSOC CREATOR/PROGRAMER it did not recognize the PSOC6 CPU
That is correct. This device is only supported in Cypress Programmer and ModusToolbox.
Could it be that the KitProg3 mode was switched by mistake?
Rakshith M B
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Rakshith
Thanks for reply.
I have to flash the simple hello world program.
when I try to flash the firmware using mbed studio in that software EVK was not detect directly so i press the switch to change the mode and EVK was detect. And able to flash the firmware properly.
but after that i am not able to flash the firmware anymore using mbed studio or modultoolbox or cypress programmer.
I have also attached error log.
Thanks & Regards
Rahul
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Rahul,
Can you please share the entire Cypress Programmer log? I see that the KitProg is detected in Cypress Programmer. Also, can you please confirm that the User LED is still blinking? To be able to use it within Mbed Studio you will have to change the mode to DAPLink. Please let me know if that works.
Rakshith M B
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
Rahul,
Have you tried using the Firmware Loader that runs within Modus Shell? Both are installed as part of ModusToolbox. Firmware loader can change the mode.
Find FW-loader in the tools directory or in the Windows start menu. FW-Loader is a program that runs in Modus Shell opened in the directory where FW-Loader resides.
With the kit plugged into your computer, type:
./fw-loader –device-list
Note: There are four modes for the kit: kp3-hid; kp3-bulk; kp3-bootloader; and kp3-daplink The different modes represent different protocols of communication.
Following are the commands to select each mode.
./fw-loader --mode kp3-hid
./fw-loader --mode kp3-bulk
./fw-loader --mode kp3-bootloader
./fw-loader --mode kp3-daplink
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content