Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 6 SDK Forum Discussions

Recent discussions

Sort by:
ricardoquesada
PSoC™ 6 SDK
Hi, TL;DR: How to know the Interrupt number that is triggered when Counter triggers a Compare or TC ?   I'm migrating a project from PSoC Creator (Sch... Show More
NovoNate
PSoC™ 6 SDK
Hello, We are developing a product that contains the CY8C6347 part using ModusToolbox v2.3.1 and we are running into issues when trying to create a bo... Show More
ravo
PSoC™ 6 SDK
Dears, when debugging project running on CY8CPROTO-062-4343W kit using KitPro3 after few minutes it stop debugging: Error: kitprog3: get_power command... Show More
micro-atama
PSoC™ 6 SDK
system stack
Solved
Hello, When I use modus,through the function uxTaskGetStackHighWaterMark(),I could confirm the task stack. But,I don't know how to comfirm the maximum... Show More
austin_h
PSoC™ 6 SDK
Hi, As title. Does CE222221 PSoC 6 MCU Voice Recorder sample code support in Modustoolbox?? I found below thread. It seems only on PSoC creater?? https://community.infineon.com/t5/PSoC-6-SDK/PSoC-62-transfer-I2S-input-to-I2S-output/m-p/170225#M211... Show More
yiru_1705901
PSoC™ 6 SDK

我现在的项目使用双核工程,M0核处理逻辑和外设,M4核只用于TFT屏刷图,,形成M0为主,M4核为从的模式。但是将cybsp_init()放在M4核运行正常,将cybsp_init()放在M0核就运行异常,请问将cybsp_init()放在M0核运行 要做哪些修改?

joshm
PSoC™ 6 SDK
ref: https://community.infineon.com/t5/AIROC-Bluetooth/MTB-PSoc6-BLE-OTA-Bootloader/m-p/330105#M1173 The example from the discussion posting above imp... Show More
joshm
PSoC™ 6 SDK
I am trying to use the example mtb-example-psoc6-mcuboot-basic on CY8CKIT-062_BLE, but I cannot get it to compile following the instructions on github... Show More
yiru_1705901
PSoC™ 6 SDK
如附件 是modus2.4操作QSPI的工程,gImage_2_2[20]这个数组没有烧录到外部flash中,读取的数据是外部flash原来的数据。 同样的代码modus2.2就操作正常,请大神帮我看下是什么问题,已经折腾我三天了。这个代码以前也是赛普拉斯AE帮我搞的,现在为了方便开发,需要移植到m... Show More
Sanyika67
PSoC™ 6 SDK
Hello, I want to use the UART with FreeRTOS using the mtb_hal_cat1 library. I use redirect_io for the printf. My question is how to enable RX interrup... Show More