Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

EdHa_4455331
Level 5
Level 5
25 replies posted 25 sign-ins 10 replies posted

I loaded up the BLE "Find Me" code example for the CYBL-416045-02 into Modus from the Git Repository.

But the projected did not include any Builders. Most other projects seem to include CDT Builder and Scan Configuration Builder.

I would add these manually, but the build diaglog doesn't seem to know anything about them and I don't know where to import

them from. So the project won't build.

Andy suggestions?

1 Solution
lock attach
Attachments are accessible only for community members.

The Find Me code example was implemented for PSoC 6 BLE Pioneer Kit. You will need to make changes for it work on the PSoC 6 BLE Prototyping Kit. For example, the code example uses RGB LEDs for BLE connection status indication. You need to use the red and green led on the kit instead.

I have made all the changes and attached it for your reference. Let me know if it works.

Regards,

Dheeraj

View solution in original post

3 Replies
DheerajK_81
Moderator
Moderator
Moderator
First comment on KBA First comment on blog 5 questions asked

Please follow this KBA to import projects correctly: Importing Code Example into ModusToolbox IDE - KBA225201

Regards,

Dheeraj

0 Likes
lock attach
Attachments are accessible only for community members.

Thank you for your prompt response. I THOUGHT that was how I did it. But I erased everything and tried again, and this time the build operation was in place. BUT…

Now I am getting errors related to the LED ports (see below) . It looks like there is a define of a define in LED.H, but the base level define cannot be found. I tried to be clever and work around this myself. I figured I could see how it was done in the Blinky project, and then use that info to repair the FindMe project. But the blinky project throws similar errors, too.

Any suggestions?

Thanks,

Ed H.

In file included from ../Source/debug.h:24:0,

from ../Source/debug.c:17:

../Source/debug.c: In function 'ShowError':

../Source/LED.h:34:32: error: 'KIT_RGB_G_PORT' undeclared (first use in this function)

#define Advertising_LED_PORT KIT_RGB_G_PORT

^

../Source/debug.c:29:19: note: in expansion of macro 'Advertising_LED_PORT'

Cy_GPIO_Write(Advertising_LED_PORT, Advertising_LED_PIN, LED_ON);

^~~~~~~~~~~~~~~~~~~~

../Source/LED.h:34:32: note: each undeclared identifier is reported only once for each function it appears in

#define Advertising_LED_PORT KIT_RGB_G_PORT

^

../Source/debug.c:29:19: note: in expansion of macro 'Advertising_LED_PORT'

Cy_GPIO_Write(Advertising_LED_PORT, Advertising_LED_PIN, LED_ON);

^~~~~~~~~~~~~~~~~~~~

../Source/LED.h:38:32: error: 'KIT_RGB_G_PIN' undeclared (first use in this function); did you mean 'KIT_RGB_G_PORT'?

#define Advertising_LED_PIN KIT_RGB_G_PIN

^

../Source/debug.c:29:41: note: in expansion of macro 'Advertising_LED_PIN'

Cy_GPIO_Write(Advertising_LED_PORT, Advertising_LED_PIN, LED_ON);

^~~~~~~~~~~~~~~~~~~

../Source/LED.h:33:28: error: 'KIT_RGB_B_PORT' undeclared (first use in this function); did you mean 'KIT_RGB_G_PORT'?

#define Alert_LED_PORT KIT_RGB_B_PORT

^

../Source/debug.c:30:19: note: in expansion of macro 'Alert_LED_PORT'

Cy_GPIO_Write(Alert_LED_PORT, Alert_LED_PIN, LED_ON);

^~~~~~~~~~~~~~

../Source/LED.h:37:27: error: 'KIT_RGB_B_PIN' undeclared (first use in this function); did you mean 'KIT_RGB_G_PIN'?

#define Alert_LED_PIN KIT_RGB_B_PIN

^

../Source/debug.c:30:35: note: in expansion of macro 'Alert_LED_PIN'

Cy_GPIO_Write(Alert_LED_PORT, Alert_LED_PIN, LED_ON);

^~~~~~~~~~~~~

../Source/LED.h:35:32: error: 'KIT_RGB_R_PORT' undeclared (first use in this function); did you mean 'KIT_RGB_B_PORT'?

#define Disconnect_LED_PORT KIT_RGB_R_PORT

^

../Source/debug.c:31:19: note: in expansion of macro 'Disconnect_LED_PORT'

Cy_GPIO_Write(Disconnect_LED_PORT, Disconnect_LED_PIN, LED_ON);

^~~~~~~~~~~~~~~~~~~

../Source/LED.h:39:31: error: 'KIT_RGB_R_PIN' undeclared (first use in this function); did you mean 'KIT_RGB_B_PIN'?

#define Disconnect_LED_PIN KIT_RGB_R_PIN

^

../Source/debug.c:31:40: note: in expansion of macro 'Disconnect_LED_PIN'

Cy_GPIO_Write(Disconnect_LED_PORT, Disconnect_LED_PIN, LED_ON);

^~~~~~~~~~~~~~~~~~

make: *** Error 1

make: *** Waiting for unfinished jobs....

In file included from ../Source/debug.h:24:0,

from ../Source/BLEFindMe.h:24,

from ../Source/BLEFindMe.c:16:

../Source/BLEFindMe.c: In function 'MCWDT_Interrupt_Handler':

../Source/LED.h:33:28: error: 'KIT_RGB_B_PORT' undeclared (first use in this function)

#define Alert_LED_PORT KIT_RGB_B_PORT

^

../Source/BLEFindMe.c:75:21: note: in expansion of macro 'Alert_LED_PORT'

Cy_GPIO_Inv(Alert_LED_PORT, Alert_LED_PIN);

^~~~~~~~~~~~~~

../Source/LED.h:33:28: note: each undeclared identifier is reported only once for each function it appears in

#define Alert_LED_PORT KIT_RGB_B_PORT

^

../Source/BLEFindMe.c:75:21: note: in expansion of macro 'Alert_LED_PORT'

Cy_GPIO_Inv(Alert_LED_PORT, Alert_LED_PIN);

^~~~~~~~~~~~~~

../Source/LED.h:37:27: error: 'KIT_RGB_B_PIN' undeclared (first use in this function); did you mean 'KIT_RGB_B_PORT'?

#define Alert_LED_PIN KIT_RGB_B_PIN

^

../Source/BLEFindMe.c:75:37: note: in expansion of macro 'Alert_LED_PIN'

Cy_GPIO_Inv(Alert_LED_PORT, Alert_LED_PIN);

^~~~~~~~~~~~~

../Source/BLEFindMe.c: In function 'BleFindMe_Process':

../Source/LED.h:33:28: error: 'KIT_RGB_B_PORT' undeclared (first use in this function)

#define Alert_LED_PORT KIT_RGB_B_PORT

^

../Source/BLEFindMe.c:220:27: note: in expansion of macro 'Alert_LED_PORT'

Cy_GPIO_Write(Alert_LED_PORT, Alert_LED_PIN, LED_OFF);

^~~~~~~~~~~~~~

../Source/LED.h:37:27: error: 'KIT_RGB_B_PIN' undeclared (first use in this function); did you mean 'KIT_RGB_B_PORT'?

#define Alert_LED_PIN KIT_RGB_B_PIN

^

../Source/BLEFindMe.c:220:43: note: in expansion of macro 'Alert_LED_PIN'

Cy_GPIO_Write(Alert_LED_PORT, Alert_LED_PIN, LED_OFF);

^~~~~~~~~~~~~

../Source/BLEFindMe.c: In function 'StackEventHandler':

../Source/LED.h:34:32: error: 'KIT_RGB_G_PORT' undeclared (first use in this function)

#define Advertising_LED_PORT KIT_RGB_G_PORT

^

../Source/BLEFindMe.c:286:31: note: in expansion of macro 'Advertising_LED_PORT'

Cy_GPIO_Write(Advertising_LED_PORT, Advertising_LED_PIN, LED_ON);

^~~~~~~~~~~~~~~~~~~~

../Source/LED.h:38:32: error: 'KIT_RGB_G_PIN' undeclared (first use in this function); did you mean 'KIT_RGB_G_PORT'?

#define Advertising_LED_PIN KIT_RGB_G_PIN

^

../Source/BLEFindMe.c:286:53: note: in expansion of macro 'Advertising_LED_PIN'

Cy_GPIO_Write(Advertising_LED_PORT, Advertising_LED_PIN, LED_ON);

^~~~~~~~~~~~~~~~~~~

../Source/LED.h:35:32: error: 'KIT_RGB_R_PORT' undeclared (first use in this function); did you mean 'KIT_RGB_G_PORT'?

#define Disconnect_LED_PORT KIT_RGB_R_PORT

^

../Source/BLEFindMe.c:287:31: note: in expansion of macro 'Disconnect_LED_PORT'

Cy_GPIO_Write(Disconnect_LED_PORT, Disconnect_LED_PIN, LED_OFF);

^~~~~~~~~~~~~~~~~~~

../Source/LED.h:39:31: error: 'KIT_RGB_R_PIN' undeclared (first use in this function); did you mean 'KIT_RGB_G_PIN'?

#define Disconnect_LED_PIN KIT_RGB_R_PIN

^

../Source/BLEFindMe.c:287:52: note: in expansion of macro 'Disconnect_LED_PIN'

Cy_GPIO_Write(Disconnect_LED_PORT, Disconnect_LED_PIN, LED_OFF);

0 Likes
lock attach
Attachments are accessible only for community members.

The Find Me code example was implemented for PSoC 6 BLE Pioneer Kit. You will need to make changes for it work on the PSoC 6 BLE Prototyping Kit. For example, the code example uses RGB LEDs for BLE connection status indication. You need to use the red and green led on the kit instead.

I have made all the changes and attached it for your reference. Let me know if it works.

Regards,

Dheeraj