Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

Anonymous
Not applicable

Whats the maximum rate at which the output of VDAC can change ? whats the maximum signal frequency i can connect to strobe?

   

 

   

thanks

0 Likes
1 Solution
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted
        In hardware input mode the VDAC8 /IDAC8 can strobe input bus up to the master clock frequency, but you may observe some artifacts on the output. Standard trick is to add 1/2 clock delay using NOT element on strobe line. Analog output frequency (sine wave) obtainable from VDAC8 without much artefacts is under 100 kHz. Adding buffer OPAMP makes it worse. The IDAC8 allows for faster output using external resistor, about 400 kHz is possible. For higher output frequencies make simple DIY R-2R DAC using 0.1℅ resistors. Such DAQ works well even at MHz frequencies.   

View solution in original post

0 Likes
2 Replies
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted
        In hardware input mode the VDAC8 /IDAC8 can strobe input bus up to the master clock frequency, but you may observe some artifacts on the output. Standard trick is to add 1/2 clock delay using NOT element on strobe line. Analog output frequency (sine wave) obtainable from VDAC8 without much artefacts is under 100 kHz. Adding buffer OPAMP makes it worse. The IDAC8 allows for faster output using external resistor, about 400 kHz is possible. For higher output frequencies make simple DIY R-2R DAC using 0.1℅ resistors. Such DAQ works well even at MHz frequencies.   
0 Likes
ViDv_264506
Level 5
Level 5
5 solutions authored First solution authored 50 replies posted

Hi, 

   

 

   

according to the PSoC5LP IDAC8 Ref B. data sheet the page 21 the Fdac update rate may be 8Msps.

   

Viktor