Hello,
I try to realize a synchronous demodulating of a signal modulated in 100khz.
I test the use of PSoc1. The use of " Modulation
Inputs " in a SCC Block seem to allow it. But I do not how see routing this input with
PSoc designer 5.3.
The routing for modulation input of SC BLOCK (generic) user module is not shown in the device editor of PSoC Designer. You need to write into AMD_CR0 or AMD_CR1 register.
For more details about this register, please refer technical reference manual of the selected device.
-Rajiv Badiger
In the TRM the section "23. Switched Capacitor PSoC Block" has the
registers you will need. Also AN2014 would be useful -
http://www.cypress.com/?rID=2899
Regards, Dana.