Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

DoFo_3472136
Level 1
Level 1

We are using the USBUART (USBFS) component in our project. It does not enumerate the same on all computers. I was wondering if anyone has seen this and if they have a possible solution? 

1 Solution
AnkitaS_51
Employee
Employee
100 likes received 50 likes received 25 likes received

The Vendor ID and Product ID fields are reported to the host computer when PSoC 3 and PSoC 5 is connected to the USB. These fields are used to ensure that the correct driver is loaded  (which is enumeration only) and the host computer application used recognizes  this project.

View solution in original post

0 Likes
1 Reply
AnkitaS_51
Employee
Employee
100 likes received 50 likes received 25 likes received

The Vendor ID and Product ID fields are reported to the host computer when PSoC 3 and PSoC 5 is connected to the USB. These fields are used to ensure that the correct driver is loaded  (which is enumeration only) and the host computer application used recognizes  this project.

0 Likes