Hi,
I have been working on a project for several days without issue and now I encounter and issue (Using Creator 3.3 S2, CY8C58XX controller).
First open project and run debug session - all ok, program compiles and parks yellow marker at start of main() ready to run
Run debugger and program executes ok.
Stop debugger and rerun, now program compiles and I see "running" status on status bar but hardware is not running. I get no opportunity to START the debug session or set a breakpoint.
If I now either make a change in code OR do a Clean and build - the debugger runs normally for this session.
If I again stop and attempt to re-run the debugger, it again does not wait for me to start the session, it shows "running" status but gardware not running and cannot stop code at a breakpoint.
Thanks
Solved! Go to Solution.
I had rarely similar issues. I usually
Bob
I had rarely similar issues. I usually
Bob
I'll try the reboot. I changed optimization to "none" in Compiler and Linker settings under the Gcc compiler. Is that all I need to remove optimisation?
Thanks again Bob
I did not mean to change any linker optimization, sorry.
Bob