Anonymous
Not applicable
Jan 17, 2010
04:32 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jan 17, 2010
04:32 PM
I want to use the 8k ECC flash to store some user information. And from the data, it seems tha the user cannot program it directly, one has to program 32 byte at a time with the orgirnal row that extra 32 bytes is linked to.
My questions is
1. Is there a way to program the those ECC flash directly?
2. If it has to program with the row that it links with, does that mean we have to copy the first 256 byte from the row into the latch and then append the 32 bytes and do a write flash?
3. Is there a way to read more than 32 byte ie say 256 byte of the ECC flash in one go?
My questions is
1. Is there a way to program the those ECC flash directly?
2. If it has to program with the row that it links with, does that mean we have to copy the first 256 byte from the row into the latch and then append the 32 bytes and do a write flash?
3. Is there a way to read more than 32 byte ie say 256 byte of the ECC flash in one go?
Labels
- Labels:
-
PSoC 3
1 Reply