Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

Hi there :

   

i am working on a project  using CY8C2966-24PVXI it's powered with 5v from regulator,it was working good without problems suddenly it started pull current up to 300 mAmp, so i removed my codes from it and reset it , now it is connected on board without code and functions but it still consumed (drawing )250mAmp and Its temperature rises rapidly , it's very hot
it is now damaged ?
what is a max current psoc1 should drawing from power supply ??

1 Reply
SampathS_11
Moderator
Moderator
Moderator
250 sign-ins 250 solutions authored 5 questions asked

The latch-up current for CY*c29466-24PVXI is 200mA, and hence the normal current drawn from the cupply should be much less. The device is damaged if the current drawn is 250mA.

0 Likes