Hi
Im trying to test an82072 but it is not stable in USB data transfer.
mostly sending the data from PC to psoc kit (CY8Ckit-001 with PSOC3 prod.) so can change the DC and not the LED state.
from time to time the opposite happens - can send but cant receive (ADC value and button state).
I'm using windows8 (tried on win7 same problem) and i also tried to update the project component but with no success.
I also tried to change the USB cable.
need help ASAP.
thanks Guy
Im using AN82072(PSoC Creator 2.1 SP1) and my board has psoc 3 prod.